How application know the model of microcontroller? Is maskset or unique numbers readable?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How application know the model of microcontroller? Is maskset or unique numbers readable?

2,027 Views
Xan
Contributor I
Hi'all, can someone tell me how to get the model of microcontroller from the application? For example, MC9S12DG256CFU maskset is 0L91N, is it in the controller's memory? What is the address of it? Or if it is not in the memory, is there any unique code in the memory i can read so that i know which controller it is.
 
 
Labels (1)
0 Kudos
Reply
2 Replies

1,100 Views
Nabla69
Contributor V
Hi Xan,
 
You can look at PARTID register in the datasheet.
It gives the model of the die inside the package.
 
Alvin.
0 Kudos
Reply

1,100 Views
Xan
Contributor I
Thanx, The location is 0x001A-1B
0 Kudos
Reply