Help needed with SCI interrupt function

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Help needed with SCI interrupt function

2,494 Views
Ryu
Contributor I
Hello.
I'm writing a program for an NE64 board, which reads a series of data over the SCI1 port, and then transmits them over the Ethernet port.
Pretty much it's done and works, but due to the amount of data collected on every reading, I have to send out 10-15 packets every time.
When the function for UDP transmission is executed, some of the data received on the serial port are skipped and lost.
I understand that in order to overcome this I need to implement an Interrupt function for the SCI1 port.
I've tried this, but my code gets stuck in an infinite loop when the SCI reading in functions takes place ( SCI1in(); ).


main.c
//***********************************
#include "RXFIFO.H"
#include "sci.h"
#include "MC9S12NE64.h"
//...and all other required files/libraries

extern void SCI1_isr_handler (void);

#pragma CODE_SEG BANKED
interrupt void SCI1Interrupt (void)
{

SCI1_isr_handler();

}
#pragma CODE_SEG DEFAULT

....





RxFifo.c
//************************************
#include "RxFifo.h"
/* Number of characters in the Fifo
the FIFO is full when it has FifoSize-1 characters */
char static volatile *RxPutPt; /* Pointer of where to put next */
char static volatile *RxGetPt; /* Pointer of where to get next */
/* FIFO is empty if PutPt=GetPt */
/* FIFO is full if PutPt+1=GetPt */
char static RxFifo[RXFIFOSIZE]; /* The statically allocated fifo data */

/*----------RxFifo_Init
Initialize fifo to be empty
Inputs: none
Outputs: none */
void RxFifo_Init(void){unsigned char SaveCCR;
/* save previous interrupt enable */
asm tpa
asm staa SaveCCR
asm sei /* make atomic */
RxPutPt=RxGetPt=&RxFifo[0]; /* Empty when PutPt=GetPt */
asm ldaa SaveCCR
asm tap /* end critical section */
}

/*---------RxFifo_Put
Enter one character into the fifo
Inputs: 8-bit data
Outputs: true if data is properly saved
Since this is called by interrupt handlers no sei,cli*/
int RxFifo_Put(char data){
char volatile *tempPt;
tempPt = RxPutPt;
*(tempPt) = data; /* try to Put data into fifo */
tempPt++;
if(tempPt == &RxFifo[RXFIFOSIZE]){ /* need to wrap?*/
tempPt = &RxFifo[0];
}
if(tempPt == RxGetPt){
return(0); /* Failed, fifo was full */
}
else{
RxPutPt = tempPt; /* Success, so update pointer */
return(1);
}
}

/*-----------------------RxFifo_Get----------------------------
Remove one character from the fifo
Inputs: pointer to place to save 8-bit data
Outputs: true if data is valid */
int RxFifo_Get(char *datapt){
if(RxPutPt == RxGetPt){
return(0); /* Empty if PutPt=GetPt */
}
else{
*datapt = *(RxGetPt);
RxGetPt++;
if(RxGetPt == &RxFifo[RXFIFOSIZE]){
RxGetPt = &RxFifo[0];
}
return(1);
}
}





sci.c
//************************************
#include
#include "ne64debug.h"
#include "MC9S12NE64.h"
#include "sci.h"
#include "RXFIFO.H"

unsigned short RxHistogram[RXFIFOSIZE]; // collected before put

void SCI1Init(void){
//Debugt("Initializing my SCI1 function\r\n");
#define ECLK 25000000 // this is BUSCLK
#define BAUD_RATE 9600
PTG_PTG2 = 0;
#define BAUD_DIV ECLK/16/BAUD_RATE

SCI1BD= BAUD_DIV;
SCI1CR1= 0;
SCI1CR2= SCI1CR2_TE_MASK | SCI1CR2_RE_MASK | SCI1CR2_RIE;
RxFifo_Init();
asm cli
}



//------SCI1 interrupt handler
interrupt void SCI1_isr_handler(void){
if(SCI1SR1 & SCI1SR1_RDRF_MASK){
RxHistogram[RxFifo_Size()]++;
RxFifo_Put(SCI1DRL); // clears RDRF
}
}


//-----Start of SCI1In
// Wait for new serial port input, return ASCII code for key typed
char SCI1In(void){

char letter;
while (RxFifo_Get(&letter) == 0){
PTG_PTG0 = 0; // Where my code stucks
};
PTG_PTG0 = 1;
return(letter);
}


My program is based on the Freescale's Connector_App, so similar initilizations take place.
I'm new at this, and I had a really hard time finding information and examples using SCI Rx interrupts. Can somebody indicate me what i'm doing wrong please?
Your help will be trully appreciated.

Thank you
Labels (1)
0 Kudos
Reply
1 Reply

1,407 Views
imajeff
Contributor III
This seems problematic to me:
Code:
#pragma CODE_SEG BANKEDinterrupt void SCI1Interrupt (void){SCI1_isr_handler();}#pragma CODE_SEG DEFAULT

 
The ISR will not like being in a banked segment, though I don't know if this is the problem you are seeing.

* I also do not see where you are enabling masked interrupts. The instruction that does it is 'cli', but I don't know if that is in some obsure macro or function in your code. If you use a debugger, finding these details would be real easy.


Message Edited by imajeff on 2007-06-27 11:06 AM
0 Kudos
Reply