Flash program and erase

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Flash program and erase

8,553件の閲覧回数
dalmeda
Contributor I

I am working flash program and erase in MC9S12DP256 controller.

 

i am not able write in flash area  , but i am using same command state machine.

 

i have attached my code give below ,i am using code worrier tool.

 

can u give some solution?

 

 progAdr=(unsigned short int *) 0xC000;
   
    bufferPtr=&buffer;
   
    FCLKDIV = 0x49;
   
    FCNFG=3;
    FSTAT_PVIOL=1;
    FSTAT_ACCERR=1;
   
    FCNFG=2;
    FSTAT_PVIOL=1;
    FSTAT_ACCERR=1;
   
    FCNFG=1;
    FSTAT_PVIOL=1;
    FSTAT_ACCERR=1;
   
    FCNFG=0;
    FSTAT_PVIOL=1;
    FSTAT_ACCERR=1;
   
    for(i=0;i<5;i++){
     
       if(FSTAT_CBEIF == 1) {
     
           *progAdr++ = *bufferPtr++;
           FCMD =0x20;
           FSTAT_CBEIF=1;
          
           if((FSTAT_PVIOL==1)||(FSTAT_ACCERR==1)) {
          
           return;
           }
       }
      
       while(FSTAT_CCIF!=1){
       }
      

ラベル(1)
0 件の賞賛
返信
16 返答(返信)

7,202件の閲覧回数
kef
Specialist I

Wrong:

 

    FSTAT_PVIOL=1;

wrong:

 

    FSTAT_ACCERR=1;

 

FSTAT register contains bits, that are cleared writing "1" to them. Since CPU can address bytes, words, but not single bits, to do FSTAT_PVIOL=1, CPU has to 1) read FSTAT, 2) do bitwise or with PVIOL bit mask, 3) write result back to FSTAT.

At 1 step CBEIF is brobably set. What happens at step 3 is you write 1 not only to PVIOL, but also to CBEIF. You are trying to launch flash command. Don't use bitfields with such flags registers.

0 件の賞賛
返信

7,202件の閲覧回数
dalmeda
Contributor I

Dear Kef,

 

Thanks for your reply,

 

FSTAT register internally create one structure .

 

That structure is contain all the bit field in code warrior header file (mc9s12dp256.h).

 

that struct assign  FSTAT address . If I want to access individual bit means directly assign to bit

 

compiler is take care  bit processing (FSTAT_PVIOL)So both are same operation.

 

Can u check attachment file?

 

In codewarrior linker file I need change any code segment address?

 

Shall I need to open any backdoor key for erasing and programming?

 

Shall I need to consider any security register?

 

--Dalmeida

 

 

 

 

0 件の賞賛
返信

7,202件の閲覧回数
kef
Specialist I

I know Codewarrior header files have bitfields defined for every register bit. But still you can't clear single flag bit properly using these bit defines. It is impossible. Any write access to such flag via bitfield structure, either flagbit=0 or flagbit=1, unavoidable write ones to flags that are set. The same applies not only to FSTAT register, but also to timer flags register, CAN status register and many other flags registers.

Again, in case CBEIF is set and you are trying to clear PVIOL or ACCERR like this FSTAT_PVIOL=1 or FSTAT_PVIOL=0 etc, you make "1" written also to CBEIF flag, because when accessing some bitfield, you have to preserve contents of "not accessed" bitfields from the same bitfields structure. CBEIF was "1", you preserve it rewriting it with "1"; so you are trying to launch some flash command.

 

Compiler can't care about hardware nuissances. I believe those bitfields should be removed from Codewarrior headers. If not all, then at least those dangerous defines for flags registers.

 

Security enabled doesn't mean flash write protection. Secured flash still can be erased/programmed from your code, so you don't need to backdoor unsecure your flash.

0 件の賞賛
返信

7,202件の閲覧回数
dalmeda
Contributor I

 

 

I have change in code  your way (byte access FAST reg),But that code also not working .

 

I have attached below code. 

 

 

unsigned short int buffer[]={0x0046,0x0047,0x0048,0x0049,0x004A}; 
  unsigned short int *progAdr;
  int i;
   
  progAdr=(unsigned short int *) 0xc000;
  
 
 
  FCLKDIV = 0x49;
 
 
  if(FCLKDIV_FDIVLD == 0){
     return;
  }
 
 
  FCNFG=3;
  FSTAT|=(PVIOL | ACCERR);
  //FSTAT_ACCERR=1;
   
  FCNFG=2;
  FSTAT|=(PVIOL | ACCERR);
  
  // FSTAT_PVIOL=1;
  // FSTAT_ACCERR=1;
  
  FCNFG=1;
  FSTAT|=(PVIOL | ACCERR);
  
  //FSTAT_PVIOL=1;
  //FSTAT_ACCERR=1;
   
  FCNFG=0;
  
  FSTAT|=(PVIOL | ACCERR);
 
 
  for(i=0;I<5;I++){
     
    if(FSTAT_CBEIF == 1) {
 
      *progAdr = buffer[i];
  
      FCMD =0x20;
 
      // (void)DoOnStack(far_address); // just passed for PPAGE
  
      FSTAT_CBEIF=1;
        if((FSTAT & PVIOL)||(FSTAT & ACCERR)) {
           return;
        }
        while(FSTAT_CBEIF == 0);
 
        progAdr++;
    }
    while(FSTAT_CCIF!=1){
    }

 
  }

 

i am using Normal Single Chip Mode in MC9S12DP256.

In Normal mode ,some registers and bits are protected

against accidental changes.

Can u confirm  u are using normal mode  or special mode?

 

 

 

 

 

 

 

 

0 件の賞賛
返信

7,202件の閲覧回数
kef
Specialist I

This is also wrong:

 

   FSTAT|=(PVIOL | ACCERR);

I don't know how PVIOL is defined in your code. Is it the defined the same like FSTAT_PVIOL_MASK from DP256  header file? It is the same like setting PVIOL and ACCERR via bitfields.

 

1) FSTAT reads with CBEIF == 1

2) you OR that with FSTAT_PVIOL_MASK and FSTAT_ACCERR_MASK

3) you write resulting value back to FSTAT with CBEIF=1. You are trying to launch flash command here!

 

 

It is not clear:

1) how does your code deal with the fact that flash memory is not readable while any flash command is being executed. That means also that you can't execute code while some flash command is in progress.

2) P&E Multilink/cyclone connection by default caches flash memory contents. Isn't it the case that program/erase succeeds but you simply see no changes in the memory? In hiwave debugger go to debugging memory map and check update memory checkbox for relevant memory blocks.

0 件の賞賛
返信

7,202件の閲覧回数
dalmeda
Contributor I

Hi kef,

 

 

 

I am tried but I am not able to launch that command.

 

can u confirm it is work in normal mode in mc9s12dp256?

 

below details are contain in  mc9s12dp256 dataseet:

 

There are two basic types of operating modes:

Normal modes — some registers and bits are protected

against accidental changes.

Special modes — allow greater access to protected control

registers and bits for special purposes such as testing.

 

 

 

 

0 件の賞賛
返信

7,202件の閲覧回数
kef
Specialist I

What's maskset of your MC9S12DP256? For example 1K79X has a bug that prevents flash and eeprom operations while chip is secured. Unsecured 1K79X is programmable in all operating modes. Other masksets that don't have these erratas are programmable and eraseable in all operating modes, both secured and unsecured.

 

Here you can find D family erratas: erratas

 

 

0 件の賞賛
返信

7,202件の閲覧回数
dalmeda
Contributor I

Hi  Kef,

 

 I have load  flash driver program in $4000 location . I need to program and erase location $8000 .

 

Is it properly work ?  I have attached my code below .

 

Please some idea kef.... 

 

  unsigned short int *progAdr; 
  int i;    
 progAdr=(unsigned short int *) 0xC000; 
  FCLKDIV = 0x49;


  FSTAT|=(FSTAT_ACCERR_MASK | FSTAT_PVIOL_MASK);

  if(FCLKDIV_FDIVLD == 0){
      return;
  }

  for(i=0;i<5;i++){
     
     if(FSTAT_CBEIF == 1) {
 
          *progAdr = 0x55;
  
           FCMD =0x20;
 
            // (void)DoOnStack(far_address); // just passed for PPAGE
  
           FSTAT |= FSTAT_CBEIF_MASK;
 
          if((FSTAT_PVIOL == 1)||(FSTAT_ACCERR == 1)) {
          return;
    }
    while(FSTAT_CBEIF == 0);
    while(FSTAT_CCIF!=1){
    }

    progAdr++;
  }
 
 
}

0 件の賞賛
返信

7,202件の閲覧回数
kef
Specialist I

1. You say you are programming 0x8000. But your code clearly uses 0xC000 as a destination address.

 

2. Programming 0x8000 with driver code at 0x4000 will succeed only for PPAGE settings <=0x3B. This is because pages 0x3C to 0x3F form single flash bank. 0x4000 belongs to PPAGE==0x3E. And code can't run in the same flash bank that is being programmed. Your code needs to execute from different flash bank, from EEPROM, from RAM or from external memory.

 

3. Programming 0xC000 with driver at 0x4000 also will fail. Because 0xC000 is PPAGE==0x3F. 0x4000 is PPAGE=0x3E. Both pages belong to the same flash bank.

 

 

4. Again, this your piece of code is WRONG:

 

  FSTAT|=(FSTAT_ACCERR_MASK | FSTAT_PVIOL_MASK);

 

^^ this code clears ACCERR, PVIOL bits and most likely writes "1' also to CBEIF, trying to launch flash command. Since FCMD is probably not loaded at this point, some error (PVIOL I think) will be triggered again. Please remove red symbol. I wrote already why bitfields are wrong. You do the same what compiler does for FSTAT_ACCERR=1 and FSTAT_PVIOL=1;. I'm afraid my explanation doesn't help you to understand why it's wrong.

 

5.  This is also not right piece of code:

 

FSTAT |= FSTAT_CBEIF_MASK;


^^ here you are not only launching flash command, but also clearing ACCERR and PVIOL.

 

 

6. Don't forget to set up BKSEL bits in FCNFG register. 00 for pages 3C to 3F, 01 for 38-3B etc.

 

 

 

After fixing these issues code should start working. Of course with restrictions specified in 2 and 3, unless you move your code to RAM.

 

0 件の賞賛
返信

7,202件の閲覧回数
dalmeda
Contributor I

Hi Kef

 

i have understand ur point and  change my code but still not working .

 

 

i have attached below .

 

 unsigned short int *progAdr;
  int i;
  progAdr=(unsigned short int *) 0x4000; 
  FCLKDIV = 0x49;
  if(FCLKDIV_FDIVLD == 0){
      return;
  }
  FCNFG=3;
  FSTAT =(FSTAT_ACCERR_MASK | FSTAT_PVIOL_MASK);

  FCNFG=2;
  FSTAT =(FSTAT_ACCERR_MASK | FSTAT_PVIOL_MASK);
  FCNFG=1;
  FSTAT =(FSTAT_ACCERR_MASK | FSTAT_PVIOL_MASK);
  FCNFG=0;
  FSTAT =(FSTAT_ACCERR_MASK | FSTAT_PVIOL_MASK); 
  for(i=0;i<5;i++){
    if(FSTAT_CBEIF == 1) {
        *progAdr = 0x41;
         FCMD =0x20;
         FSTAT = FSTAT_CBEIF_MASK;
        if((FSTAT_PVIOL == 1)||(FSTAT_ACCERR == 1)) {
           return;
       }
       while(FSTAT_CBEIF == 0);
       progAdr++;
   }
 
}
  while(FSTAT_CCIF!=1){} 
  

 

 Start_up code available in Unbanked Flash ROM $C000

 

 flash driver program available in banked Flash ROM $30  to $3D

i am trying write  at unbanked ROM  S4000 .Is it possible?

 

Can u confirm it is working or not?

 

Please refer attachment file 

 

Can u give some solution?   
 

0 件の賞賛
返信

7,202件の閲覧回数
kef
Specialist I

Your code is working. But programming 0x4000, driver code can not be placed in pages 0x3C..0x3F, because 0x4000 and pages 3C..3D are flash bank0.

Alsoo since interrupt vectors at 0xFFxx also to bank0, you should disable interrupts while erasing/programming.

 

Did you make debugger updating flash at 0x4000? HCSMultilinkCyclonePro->Debugging Memory Map...->Unbanked Flash 4000->refresh memory when halting?

0 件の賞賛
返信

7,202件の閲覧回数
dalmeda
Contributor I

Dear Kef,

 

 

 

shall I need to add any code after command processing ?

 

In our code after command processing illegal_BP error is send

 

but that data is write in flah.how to handle this problem ?  

 

 

 

 

 

0 件の賞賛
返信

7,202件の閲覧回数
kef
Specialist I

It succeeds without illegal_BP. Did you change addresses and forgot about restrictions that program/erase routines can't program bank-N and execute from the same bank-N? Did you disable interrupts?

0 件の賞賛
返信

7,202件の閲覧回数
dalmeda
Contributor I

Hi Kef,

 

I have disable  all the interrupt.  I have changed location also .

 

Still that program is problem(illegal_BP)  in execution time

 

 i  have attached my program below .this program stored in $30 area.i  am using same lier file 

 

 unsigned short int *progAdr;
  int i;
 progAdr=(unsigned short int *) 0xD000; 
 DisableInterrupts;
 FCLKDIV = 0x49;
 if(FCLKDIV_FDIVLD == 0){
      return;
 }
 FCNFG=3;
 FSTAT =(FSTAT_ACCERR_MASK | FSTAT_PVIOL_MASK);

 FCNFG=2;
 FSTAT =(FSTAT_ACCERR_MASK | FSTAT_PVIOL_MASK);
 FCNFG=1;
 FSTAT =(FSTAT_ACCERR_MASK | FSTAT_PVIOL_MASK);
 FCNFG=0;
 FSTAT =(FSTAT_ACCERR_MASK | FSTAT_PVIOL_MASK);

  
  for(i=0;i<5;i++){
    if(FSTAT_CBEIF == 1) {
       *progAdr = 0x4141;
        FCMD =0x20;
         FSTAT = FSTAT_CBEIF_MASK;
   
    if((FSTAT_PVIOL == 1)||(FSTAT_ACCERR == 1)) {
       return;
    }
    while(FSTAT_CBEIF == 0);
    progAdr++;
  }
 
}
while(FSTAT_CCIF!=1){}

 

 

0 件の賞賛
返信

7,202件の閲覧回数
kef
Specialist I

Dalmeda,

 

I tried myself your code from the previous message. It is working. Period. I don't know what are you doing it doesn't work for you. It worked in both special and notmal single chip modes.

0 件の賞賛
返信

7,202件の閲覧回数
dalmeda
Contributor I

Dear Kef,

 

Its working in RAM when I need launch the program and erase command . 

 

 

Thanks for giving your wonderful support and your time.

 

 

 

0 件の賞賛
返信