Flash data retention of S12ZVM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Flash data retention of S12ZVM

806 次查看
ikkishingu
Contributor II

Hello,

 

Please tell me the interpretation of Flash data retention of S12ZVM.

 

There is the description on S12ZVM RM Table F-5 as below

Data retention at an average junction temperature of TJavg = 85°C(1)

after up to 10,000 program/erase cycles tNVMRET : min 20 years, typ 100 years

 

I translate this description literally, then I can understand the contents as below,

1. At first, S12ZVM Flash is programed/erased 10,000 cycles at Freescale test sites.

2. After 1., Freescale tests the data retention time using "the ragged Flash" with the threshold equivalent 20 years by Arrhenius equation.

 

It is not natural for me, however is my understanding correct?

 

Best Regards,

Ikki

标签 (1)
标记 (1)
0 项奖励
回复
0 回复数