FLAT8000_P30 memory

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,114件の閲覧回数
michaelsarafidi
Contributor II

hi there,

 

We are using HC12DG256  and Codewarrior 3.1. These days we are evaluating Codewarior 5.1.

We have opened our project with CW 5.1 built it and run it successfully.

 

What i want to ask is what is FLAT8000_P30 or flash window (memory from 0x8000 to 0xBFFF).

At CW3.1 this area was empty (0xFF), at CW5.1 is full.

 

Thanks in advance.

 


ラベル(1)
1 解決策
2,021件の閲覧回数
RadekS
NXP Employee
NXP Employee

At address 0x8000 to 0xBFFF is flash memory window.

S12DG256 is 16bit MCU, therefore we can directly address only 64kB memory range (0x0000~0xFFFF).

S12DG256 contain 256kB flash, this flash is divided to sixteen 16kB pages (page 30~3F). We can access whole flash trough memory window. At address 0x8000 to 0xBFFF is visible page content according PPAGE register settings. Two pages (3E, 3F) are accessible directly (0x4000~0x7FFF, 0xC000~0xFFFF) and we call them as non-banked.

Default placement for your code is paged flash (banked). Therefore you see your code at page 30.

For details, please check your project *.prm file. Placement of your code you can drive by #pragma commands (for example):

#pragma CODE_SEG NON_BANKED

//your code

#pragma CODE_SEG DEFAULT


元の投稿で解決策を見る

2 返答(返信)
2,022件の閲覧回数
RadekS
NXP Employee
NXP Employee

At address 0x8000 to 0xBFFF is flash memory window.

S12DG256 is 16bit MCU, therefore we can directly address only 64kB memory range (0x0000~0xFFFF).

S12DG256 contain 256kB flash, this flash is divided to sixteen 16kB pages (page 30~3F). We can access whole flash trough memory window. At address 0x8000 to 0xBFFF is visible page content according PPAGE register settings. Two pages (3E, 3F) are accessible directly (0x4000~0x7FFF, 0xC000~0xFFFF) and we call them as non-banked.

Default placement for your code is paged flash (banked). Therefore you see your code at page 30.

For details, please check your project *.prm file. Placement of your code you can drive by #pragma commands (for example):

#pragma CODE_SEG NON_BANKED

//your code

#pragma CODE_SEG DEFAULT


2,021件の閲覧回数
GordonD
Contributor IV

Michael,

Where are you seeing the text "FLAT8000_P30" in the .map file? In the .prm file?

Regards,

Gordon

0 件の賞賛
返信