External memory and peripherals

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

External memory and peripherals

2,125件の閲覧回数
lotfiB
Contributor I
I want a mode of HCS12 to have the following configuration:
1- Use the internal memory map including registers, eeprom, ram and a part of (no)banked-flash, as in normal single chip.
2- Add an external parallel RAM device, for example 1 Megabyte (20 bits) for aquisition data storage.
3- Add an external parallel peripheral such an ADConverter, 12 bits resolution .
 
The control of these elements must be done by external bus, not by I/O ports.
The internal flash must visible for loading and execution program .
I read very quicly appliaction note AN2408, is it a good beginning?
Thanks
ラベル(1)
0 件の賞賛
返信
1 返信

1,181件の閲覧回数
Alban
Senior Contributor II
Hello,
 
This is not possible with an S12.
The external bus has the S12 as a Master.
 
Alban.
0 件の賞賛
返信