Error while re-transmitting data via CAN between two MC9S12XEP100

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Error while re-transmitting data via CAN between two MC9S12XEP100

2,023件の閲覧回数
harshal_pawar
Contributor III

I am working on establishing communication between two MC9S12XEP100 controllers using CAN MAX3050ASA+ interface.

Case 1:

The data is transmitted on key press event from First board and received using interrupt at second board and it also displayed on GLCD display (Display is at Secondary side)

Its working fine.

Case 2:

When I updated the same code for receiving data at second board and re-transmitting it to first board neither values are updating on display nor receiving at Tx side (i.e. first board).

Code Workflow for Case 1:

At Tx:

1. In infinite loop check for key press event

2. If Yes, the Check for empty buffer

3. Select empty buffer

4. Create message

5. Make Buffer Ready

6. Check transmission status

At Rx:

1. In receive ISR, get the data transmitted from first board & display it on GLCD

Code Workflow for Case 2:

At Tx:

Step 1 to 6 are same

7. Receive ISR for the re-transmitted data from second borad

At Rx:

1. In receive ISR get the data transmitted from first board & display it on GLCD

2. Re-transmit the same data as an acknoledgement as per following steps:

3. Check for empty buffer

4. Select empty buffer

5. Create message

6. Make Buffer Ready

7. Check transmission status

ラベル(1)
0 件の賞賛
返信
1 返信

1,909件の閲覧回数
harshal_pawar
Contributor III

The issue has been resolved. There was a mistake in code. Now the system is working fine.

0 件の賞賛
返信