EEPROM & Flash lifespans

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

EEPROM & Flash lifespans

2,414 Views
Dr_Colloid
Contributor I
We are working on a new version of our instrument that will use a Freescale MC9S12DP512 MCU. In the Device User Guide, there is a table indicating that over the operating range of -40C to 125C, the NVM Reliability Characteristics, which we aren't sure if we're even interpreting correctly are:

Flash: Data Retention of 15 years if the memory is cycled 10 times.
EEPROM: Data Retention of 15 years if only cycled 10 times, dropping to 5 years if the EEPROM is cycled 10000 times.

Out instruments have had useful lives of 20-25 years, so a 15 year life is worrying. Further, we are saving use settings in EEPROM that can change daily, and a 5 year life there is even more of a problem. On the other hand, the instrument is used in a laboratory setting over comfortable room temperatures, not at the extremes of 125C and -40C. Is there more detailed information on this subject available somewhere?

Thanks.
Labels (1)
0 Kudos
Reply
1 Reply

1,211 Views
Nabla69
Contributor V
Dear Dr. C,
 
You have special Engineering Bulletins describing how Freescale came up with these numbers:
 
 
If you work at room temperature, the cycling before failure was measured but NOT guaranteed at several millions program/erase cycles.
I imagine your instruments don't spend their time modifying the EEPROM.
In this case I am totally confident in a 25 years life.
 
Freescale Flash/EEPROM specifications might sound worrying compared to competitors... But Freescale does guarantee the values across the FULL temperature RANGE. Not all of them do !
 
Cheers,
Alvin.
0 Kudos
Reply