EEPROM Emulation for MC9S12C32

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

EEPROM Emulation for MC9S12C32

3,376件の閲覧回数
EEstudent
Contributor I
Does anyone have any example code for emulating EEPROM on a MC9S12C32?  This has been stumping my microcontroller applications teacher and myself.  Any help what-so-ever would be greatly appreciated.  If I show your code to my instructor, you will be cited.  He encourages us to scour the web for help if we get stuck.  I am definately stuck.  Thanks... 
ラベル(1)
0 件の賞賛
返信
4 返答(返信)

1,901件の閲覧回数
DPB
NXP Employee
NXP Employee
Hello

The AN2302  is  written specifically for EE emulation on the MC9S12C32 http://www.freescale.com/files/microcontrollers/doc/app_note/AN2302.pdf?fsrch=1&WT_TYPE=Application%...

This also includes code examples.

DPB
0 件の賞賛
返信

1,901件の閲覧回数
JimDon
Senior Contributor III
You need AN2204 "Fast NVM Programming for the MC9S12DP256" and the SW file for it.

This is sample code to program flash.

Here is a link, look down the page.


0 件の賞賛
返信

1,901件の閲覧回数
EEstudent
Contributor I
Thanks, I'll go take a look at it right now.
0 件の賞賛
返信

1,901件の閲覧回数
allawtterb
Contributor IV
I would also suggest taking a look at AN2720, this AN is a bit more recent than the one Jim referenced.
 
 
- Brett
0 件の賞賛
返信