Do we need admin/elevated access for flashing using Codewarrior ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Do we need admin/elevated access for flashing using Codewarrior ?

1,790 Views
in-nitin-gupta
Contributor I

Hi

I am trying to perform remote flashing using TCL script triggered through batch file. 

Whenever I try to execute without elevated/admin access, CW opens but no further execution whereas it works if triggered with admin access.

Just wanted to know that is it mandatory to trigger that way or some work around ? 

Tags (1)
0 Kudos
Reply
1 Reply

1,689 Views
jiri_kral
NXP Employee
NXP Employee

Hi,

I'm not much familiar with TCL and CW flashing tools, but it looks that for some HW communication are escalated privileges required. 

Other possibility is that the tool is installed to the path with restricted access. 

0 Kudos
Reply