DSP56858 Bootstrap from SCI

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DSP56858 Bootstrap from SCI

1,650 Views
ChrisMorgan
Contributor I
Can anyone point me toward directions for the bootstrap from SCI (mode 6) for the DSP56858 processor?  The information in the user manual and datasheets is very limited.  I have sent a lot of data to the DSP but I don't see any feedback from the bootstrap - which is understandable since it is a very compact piece of code.
Labels (1)
0 Kudos
Reply
1 Reply

1,191 Views
dbrown
Contributor I

Chris,

 

I've just had the exact same problem and even a service request didn't solve my problem.

However, I figured it out... also on the DSP56858.

 

I created a new project using the example stationary for an internal bootloader and built it for the correct processor. You then have to pass this output file through Freescale's "srec_to_boot_format.exe" file in your C:\Program Files.... folder. This must be a binary file though. I've attached my subsequent binary file if it helps.

 

The micro then needs powering up and the file sending through hyperterminal (within 3 sec in my case) at 38400,8,N,1 (no flow control) by using Send text file, not send file. If you're using teraterm then make sure you tick the "binary" check box.

 

When this is sent you will receive "OK" in return, don't power down as it is now in bootmode and then send your output file for your actual project. If you don't get "OK" then no point continuing...

 

One final thing is MODA should be tied low, MODB and MODC to Vdd.

 

Hope this helps...

0 Kudos
Reply