Codewarrior 3.1 & windows 8.1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Codewarrior 3.1 & windows 8.1

1,515 Views
Eric_t
Contributor III

Hi everybody,

 

I used to work with codewarrior 3.1 and windows XP.

Now I have been given a PC with Windows 8.1

Unfortunately CW does not work; when CW starts an error occurs:

A problem caused the program to stop working correctly.

Windows will close the program and notify you if a solution is available.

 

Also compatibility with Win XP does not help

Does anyone know if there is any way to make CW 3.1 to work win Win 8.1 or I have to go back to Win XP?

 

Thank you

 

 

Labels (1)
0 Kudos
Reply
1 Reply

1,165 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

hello Eric.

CW3.1 is a very old version. it can be supported by 32bit 2000/xp, but can't win7/win8.

so far we only have CW5.1 can support 32/64bit win7 but no CW for HCS12 version can support win8.1

here is CW5.1:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-HCS12X

if you insist using CW3.1, please stay on 32bit xp computer. if you use USB multilink interface . you need also install CodeWarrior for HC12 v3.1 - USB 2.0 Service Pack

http://www.freescale.com/webapp/sps/site/overview.jsp?code=CW_UPDATES_HCS12_31

===============================================

this answer is for you. if it helps, please click on "correct answer" button. thanks!

Best Regards,

ZhangJun

0 Kudos
Reply