Clearing the bit

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Clearing the bit

4,465 Views
admin
Specialist II
Hello All,
               My doubt is that in certain microcontrollers like MPC5554 ,certain bits are cleared by writing a '1' on it .Why is it so? Normally bits are cleared by  writing a '0'. 
Labels (1)
0 Kudos
Reply
7 Replies

2,426 Views
admin
Specialist II
Hello All
             Thank you for your kind information.
         
0 Kudos
Reply

2,427 Views
admin
Specialist II
Hello All
              I dont know whether everyone understood my doubt,Lets consider this bit in register

EQADC_FISRn of MPC5554.

EOQFn End-of-queue flag n. Indicates that an entry with an asserted EOQ bit was transferred from CFIFOn to the on-chip ADCs or to the external device. . When the eQADC

completes the transfer of an entry with an asserted EOQ bit from CFIFOn, EOQFn will be

set. Writing a 1 clears the EOQFn bit. Writing a 0 has no effect.

0 Entry with asserted EOQ bit was not transferred from CFIFOn

1 Entry with asserted EOQ bit was transferred from CFIFOn.

How again writing a "1" clears that bit ?

0 Kudos
Reply

2,426 Views
kef
Specialist I
Probably there's something like FISRn trigger, AND gate and "chip select" circuit, all wired so that when EQADC register is selected and WRite is high and data bus bit corresponding to FISRn bit position is '1', then FISRn trigger is reset. Simple.
 
BTW MPC5554 is not a 16bits MCU.
0 Kudos
Reply

2,426 Views
Lundin
Senior Contributor IV
Because Freescale refrains from making their mcu peripherals logical and intuitive whenever possible...

Clear by writing 1 or clear by reading are very annoying features of some peripherals, that surely must cause millions of bugs for all Freescale users, especially those who are using C. I bet every single user sooner or later runs into classic Freescale bug 1: "the debugger is eating my SCI/SPI flags" and classic Freescale bug 2: "my timer flags are destroyed because I clear a flag with TIMER_REG |= 0x01 rather than TIMER_REG = 0x01".

But the C language has only been standardized for 18 years, so if we give Freescale more time they might at some point adapt their micros to support this new fancy language.
0 Kudos
Reply

2,426 Views
kef
Specialist I
Lundin,
this issue isn't easy to fix. Would you like slowing down CPU like it's done in Microchip MCUs to solve this? Maybe slowing down peripherals? More complicated circuit and more expensive chip? One flag per register leading to more address space occupied by registers block (something like in S08 family, but first compare how many flags does S12D family have)? I wouldn't.
Egg vs chicken. Is C more important than everything else?
 
0 Kudos
Reply

2,426 Views
Lundin
Senior Contributor IV
Changing logic level from 1 to 0 can hardly be expensive. The clear-by-read issues in SCI/SPI are seem to be there for backwards compatibility only.

Another case where the C language has clearly not been considered is the address map. A write to address zero should yield an error interrupt on a micro designed for the C language, to prevent null pointer access.

Also, companies like Freescale spend huge amounts of cash on things like AUTOSAR to reduce software bugs. In my opinion they should start fixing the simple things first.
0 Kudos
Reply

2,426 Views
kef
Specialist I
You don't like NOTsimple change of logics from 1 to 0, do you? Let's think about timer flags. Currently, to clear bit0 and keep other bits in their current state you write
 
TFLG1 = 1;
 
After change of logics 1->0, above would become
 
TFLG1 = 0xFE;
 
But neither
  
    TFLG1 &= ~1; // (BCLR TFLG1,#1)
 
nor
 
     TFLG1_C0F=0; // (also BCLR TFLG1,#1)
 
would work properly! Both variants would clear more bits than you expect!
And backwards compatibility is another issue non issue.
0 Kudos
Reply