Can't find USB BDM Tool driver

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can't find USB BDM Tool driver

2,635件の閲覧回数
thomaskoger
Contributor I

I just got the KIT912S812ECUEVM reference design kit.  There are no instructions on where to download the driver for the USB dongle.

ラベル(1)
0 件の賞賛
返信
5 返答(返信)

2,188件の閲覧回数
Martin35804
NXP Employee
NXP Employee

Hi,

The TBDML drivers can be found at sourceforge portal.

Check the following post at Freescale community:

https://community.freescale.com/thread/307079

This should help.

0 件の賞賛
返信

2,188件の閲覧回数
thomaskoger
Contributor I

I tried the drivers listed there, but I get an error message saying "This device cannot start. (Code 10)"

0 件の賞賛
返信

2,188件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

according to CW5.1 release note. CW5.1 doesn't support TBDML under 64bit windows. see attached Notes_CW_HC12_64bit.txt.

we can also find this file under {CW5.1 install}\Release_Notes\HC12

if user use win7 system, we suggest use CW5.1 with BDM multilink interface. You can check USB BDM Multilink Cable in this url:
(http://www.pemicro.com/products/product_viewDetails.cfm?product_id=33&CFID=8162137&CFTOKEN=8f9727e0d... )


Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,188件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Thomas,

do you mean driver for USB BDM tool? there is no special drive for it.

Installation will be required if this is the first connection to the PC, follow on screen menu and install driver automatically.

check windows device manager if it can well recognize it.


Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,188件の閲覧回数
thomaskoger
Contributor I

Hi Zhang,

windows 7 does not recognize this device, so can't find a driver.

-Tom

0 件の賞賛
返信