CAN Acceptance Filters usage for MC9S12XEP100CVL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CAN Acceptance Filters usage for MC9S12XEP100CVL

1,727 Views
sushantbanavali
Contributor I

Hello,

I am working on an automotive  prototype project where CAN messages are read over 16 bit MC9S12XEP100CVL.

The CAN message format is standard 11bit idenfier.

I am interested in receiving CAN messages in the range of 0x300 to 0x600.

Kindly let me know how acceptance filters can be applied to filter the above range. 

4 Replies

1,233 Views
lama
NXP TechSupport
NXP TechSupport

Hi,

I would like to add....

Having read the question I have found you wanted to filter ID up to 0x600. I suppose it is not 0x600 but 0x5FF. Do not hesitate to response if following is not clear.
If it is 0x5FF then set the filter 3 (CANIDAR67,CANIDMR67) in the same way as any of the previous filters. It means, for example, CANIDAR67 will be set as CANIDAR45 and CANIDMR67 will be set as CANIDMR45.

However, if you want exactly interval from 0x300 to ox600 the filter 0,1,2 are OK but the last filter, filter 3, should be set for exact value 0x600 which means:

A) both data and remote frames and standard identifiers only

// filter3 setup - the exact value 0x600 filter, both data and remote frames are accepted

CANIDAR6 = 0B11000000; // ID10,9,8,7,6,5,4,3

CANIDAR7 = 0B00000000; // ID2,1,0,RTR,IDE,x,x,x  (1/0=ignore/match)

CANIDMR6 = 0B00011111; // ID10,9,8,7,6,5,4,3

CANIDMR7 = 0B00010111; // ID2,1,0,RTR,IDE,x,x,x (1/0=ignore/match).... ignore data/remote, match standard only frame

B) The setup accepts ID within range 0x300-0x600 for data frames only and standard identifiers only

// filter3 setup - the exact value 0x600 filter, data frames are only accepted

CANIDAR6 = 0B11000000; // ID10,9,8,7,6,5,4,3

CANIDAR7 = 0B00000000; // ID2,1,0,RTR,IDE,x,x,x  (1/0=ignore/match)

CANIDMR6 = 0B00000000; // ID10,9,8,7,6,5,4,3

CANIDMR7 = 0B00000111; // ID2,1,0,RTR,IDE,x,x,x (1/0=ignore/match).... match data only, match standard only frame

 Is it clear?

Best regards,

Ladislav

0 Kudos
Reply

1,233 Views
sushantbanavali
Contributor I

Hello Ladislav,

Thanks for the information.I have successfully applied the above filters to allow messages from 0x300 to 0x600.

0 Kudos
Reply

1,233 Views
lama
NXP TechSupport
NXP TechSupport

Hi,

because of given range you should use 4z16bit filter setup as follows.

I hope I have not made a mistake.

A) The setup accepts ID within range 0x300-0x6FF for both data and remote frames and standard identifiers only

CANIDAC = 0b00010000;   // select 4x16bit filters

// filter0 setup - range 0x300-0x3FF, both data and remote frames are accepted

CANIDAR0 = 0B01100000; // ID10,9,8,7,6,5,4,3

CANIDAR1 = 0B00000000; // ID2,1,0,RTR,IDE,x,x,x  (1/0=ignore/match)

CANIDMR0 = 0B00011111; // ID10,9,8,7,6,5,4,3

CANIDMR1 = 0B11110111; // ID2,1,0,RTR,IDE,x,x,x (1/0=ignore/match).... ignore data/remote, match standard only frame

// filter1 setup - range 0x400-0x4FF, both data and remote frames are accepted

CANIDAR2 = 0B10000000; // ID10,9,8,7,6,5,4,3

CANIDAR3 = 0B00000000; // ID2,1,0,RTR,IDE,x,x,x  (1/0=ignore/match)

CANIDMR2 = 0B00011111; // ID10,9,8,7,6,5,4,3

CANIDMR3 = 0B11110111; // ID2,1,0,RTR,IDE,x,x,x (1/0=ignore/match).... ignore data/remote, match standard only frame

// filter2 setup - range 0x500-0x5FF, both data and remote frames are accepted

CANIDAR4 = 0B10100000; // ID10,9,8,7,6,5,4,3

CANIDAR5 = 0B00000000; // ID2,1,0,RTR,IDE,x,x,x  (1/0=ignore/match)

CANIDMR4 = 0B00011111; // ID10,9,8,7,6,5,4,3

CANIDMR5 = 0B11110111; // ID2,1,0,RTR,IDE,x,x,x (1/0=ignore/match).... ignore data/remote, match standard only frame

// filter3 setup - range 0x600-0x6FF, both data and remote frames are accepted

CANIDAR6 = 0B11000000; // ID10,9,8,7,6,5,4,3

CANIDAR7 = 0B00000000; // ID2,1,0,RTR,IDE,x,x,x  (1/0=ignore/match)

CANIDMR6 = 0B00011111; // ID10,9,8,7,6,5,4,3

CANIDMR7 = 0B11110111; // ID2,1,0,RTR,IDE,x,x,x (1/0=ignore/match).... ignore data/remote, match standard only frame

B) The setup accepts ID within range 0x300-0x6FF for data frames only and standard identifiers only

CANIDAC = 0b00010000;   // select 4x16bit filters

// filter0 setup - range 0x300-0x3FF, data frames are only accepted

CANIDAR0 = 0B01100000; // ID10,9,8,7,6,5,4,3

CANIDAR1 = 0B00000000; // ID2,1,0,RTR,IDE,x,x,x  (1/0=ignore/match)

CANIDMR0 = 0B00011111; // ID10,9,8,7,6,5,4,3

CANIDMR1 = 0B11100111; // ID2,1,0,RTR,IDE,x,x,x (1/0=ignore/match).... match data only, match standard only frame

// filter1 setup - range 0x400-0x4FF, data frames are only accepted

CANIDAR2 = 0B10000000; // ID10,9,8,7,6,5,4,3

CANIDAR3 = 0B00000000; // ID2,1,0,RTR,IDE,x,x,x  (1/0=ignore/match)

CANIDMR2 = 0B00011111; // ID10,9,8,7,6,5,4,3

CANIDMR3 = 0B11100111; // ID2,1,0,RTR,IDE,x,x,x (1/0=ignore/match).... match data only, match standard only frame

// filter2 setup - range 0x500-0x5FF, data frames are only accepted

CANIDAR4 = 0B10100000; // ID10,9,8,7,6,5,4,3

CANIDAR5 = 0B00000000; // ID2,1,0,RTR,IDE,x,x,x  (1/0=ignore/match)

CANIDMR4 = 0B00011111; // ID10,9,8,7,6,5,4,3

CANIDMR5 = 0B11100111; // ID2,1,0,RTR,IDE,x,x,x (1/0=ignore/match).... match data only, match standard only frame

// filter3 setup - range 0x600-0x6FF, data frames are only accepted

CANIDAR6 = 0B11000000; // ID10,9,8,7,6,5,4,3

CANIDAR7 = 0B00000000; // ID2,1,0,RTR,IDE,x,x,x  (1/0=ignore/match)

CANIDMR6 = 0B00011111; // ID10,9,8,7,6,5,4,3

CANIDMR7 = 0B11100111; // ID2,1,0,RTR,IDE,x,x,x (1/0=ignore/match).... match data only, match standard only frame

In detail you can see it here,

pastedImage_2.png

Best regards,

Ladislav

1,233 Views
aaronlee
Contributor V

Hi, Ladislav,

Why the RTR in CANIDAR1, 3, 5 & 7 are different ?

pastedImage_1.png

Best Regards,

Aaron

0 Kudos
Reply