Bootloader for Serial (UART) flashing of MC9S12xDP512

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Bootloader for Serial (UART) flashing of MC9S12xDP512

跳至解决方案
3,665 次查看
santhoshsl
Contributor III

Hello All,

 

we are using MC9S12xDP512 controller for our project. Currently we are using Softec and P&E tools to flash our .s19 files.

But we need to develop an UI or application for PC which communicated through UART to our controller and this Application will have options to read and write FLash or EEProm.

So can you please let me know if there are any bootloaders (open source) available for this flashing through UART.

标签 (1)
标记 (2)
0 项奖励
回复
1 解答
2,911 次查看
RadekS
NXP Employee
NXP Employee

In attachment you can find slightly modified Gordon’s bootloader include short introduction, conversion tool and demo application.

I hope it helps you.

在原帖中查看解决方案

0 项奖励
回复
4 回复数
2,911 次查看
GordonD
Contributor IV

Santhosh,

I've attached a CW Classic project for an S12XDP512 bootloader that I wrote a number of years ago. No guarantees, but the code is fairly well commented.

Best Regards,

Gordon

2,911 次查看
santhoshsl
Contributor III

Hello Gordon,

Thanks for your code. Its nice and giving me direction to code for my requirement. I am going through code and once I test the same, will let you know the update.

I was out of station for few days, so the delay in my response. Sorry for this.

Regards

Santhosh S L

0 项奖励
回复
2,912 次查看
RadekS
NXP Employee
NXP Employee

In attachment you can find slightly modified Gordon’s bootloader include short introduction, conversion tool and demo application.

I hope it helps you.

0 项奖励
回复
2,911 次查看
santhoshsl
Contributor III

Hello Radek,

Thanks for this support and sorry for delay in my reply (had not internet connection for few days).

I have compiled the code and will test the same and let you guys know the update.

Regards

Santhosh S L