About MC9S12Dx512's MMC-Memory-map file.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About MC9S12Dx512's MMC-Memory-map file.

3,711件の閲覧回数
yongpanan
Contributor II

HI

I am now doing a bootloader based on the MC9S12DP512, but now I have  some problems. Flash on the use of the time to use the address, I should use the global address or PPAGE configuration selection erase it. Can you give me a memory map? There is no single-chip internal address register? I can not find the relevant introduction in the chip manual.

ラベル(1)
0 件の賞賛
返信
4 返答(返信)

3,473件の閲覧回数
lama
NXP TechSupport
NXP TechSupport

Hi,

there is no globla memory approach. In order to be access any part of the flash you can use 16bit address only for spaces 4000~7FFF and C000~FFFF which are also addressable via PPAGE access via pages 3E and 3F together with window 8000~BFFF.

Moreover, the memory map can be affected by modification registers INITRG, INITRM and INITEE.

The memory map can be found in the attachment.

Moreover, I have attached a SW which can help you to create your own bootloader.

Best regards,

Ladislav

3,472件の閲覧回数
yongpanan
Contributor II

Thanks,
About the An3275SW ,Can I used for MC9S12DP512 directly?
If no,Which module did i should to modify?
I was the first to use this chip。And the AN3275SW is too diffcult for me to understanding.

0 件の賞賛
返信

3,473件の閲覧回数
lama
NXP TechSupport
NXP TechSupport

Hi,

yes, you can us it directly. However, it is necessary to read the entire AN3275.pdf carefully.

Best reards,

Ladislav

0 件の賞賛
返信

3,473件の閲覧回数
yongpanan
Contributor II

Got it.

Thank you.

0 件の賞賛
返信