About Flash Download Speed---XHY256

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About Flash Download Speed---XHY256

1,008件の閲覧回数
StoneSun
Contributor I

Dear all:

   Does anyone mets this problem:use P&E's Multilink 2.0 for XHY256 Flash download the speed is only about 3.3K. When i use the DEMO9S12XHY256 Board download the same project the speed is about 6K! What's the problem? The XHY256 Chip OR the multilink?   Thanks!

  Another question: How Can i use the Demo Board's debugger?Someone said must change the dll file of cw or only the CW 6.2 ssupport the function.And i know the on board debugger has it's own version&ID. Is this the point? I can change the version & ID by hardware.How Can i use it? I have Two Demo Board & i do not want to spend any money on another P&E's BDM debugger!

ラベル(1)
0 件の賞賛
返信
0 返答(返信)