About Cyclone and USBMULTILINKBDM difference

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About Cyclone and USBMULTILINKBDM difference

3,406件の閲覧回数
lijiandong
Contributor I

I have heard someone said that USBMULTILINKBDM isn't full function in 9S12 debugging, in some case, when the chip was  in wrong  BDM status, the USBMULTILINKBDM can't connect to the target board,need the cyclone to renable the chip  for USBMULTILINKBDM connecting, I am confused to this problem,I have encountered several times,

Could you please to expound?

Thanks

ラベル(1)
0 件の賞賛
返信
1 返信

1,248件の閲覧回数
alex_spotw
Contributor III
Hi:

In some conditions or if you explicitly do so, the HCS12 becomes 'secured' and the USB BDM cannot communicate anymore. In that case you need to use the 'unsecure12' program to unsecure the device. After that, the BMD will recognize it again.

You can download the unsecure12 program from the P&E Micro website.

Regards,

Alex
0 件の賞賛
返信