9S12NE64 and USB-LAN adapter problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

9S12NE64 and USB-LAN adapter problem

877 Views
kumle
Contributor I

My Laptop has no network card and I bought USB-LAN adapter SR9600 , BUT my demo board is NOT CONNECTED to this network card !!!

I checked out the demo board from contacting the usual network card on my Desktop everything works fine.

I have disabled the autonegotiation and use 10baseT mode.

 

I load the project from the CD to the demo board NE64_OpenTCP.mcp

 

I debug the program step by step and see that the variable  gotlink is 0.

And I see that the interrupt from ethernet controller does not occur even if I connect or disconnect the LAN cord.

 

Moreover my USB-LAN adapter properly connected to the my Desktop !!!

 

usb-lan link:

http://www.dealextreme.com/feedbacks/BrowseReviews.dx/sku.2797

 

what's to do ?

Labels (1)
0 Kudos
Reply
0 Replies