Questions regarding BMS: RDDRONE-BMS772

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Questions regarding BMS: RDDRONE-BMS772

2,791 次查看
sbi
Contributor I

Hello,

We have questions regarding the BMS: Smart Battery Management for Mobile Robotics | NXP Semiconductors for drone applications.

1. Does the device have a clock in the format year/month/day (uint8/uint8/uint8 YY/MM/DD)?

2. UAVCAN packet structure? -> We intend to connect the device to a Single Board Computer (eg Raspberry)

3. Firmware latest release BMS5.0 @GitHub: Is this version production ready or does it need additional programming? Or should we change only some values depending on our requirements in the parameters from the command line?
 
Thank you in advance.
0 项奖励
回复
0 回复数