What is the correct offset for u-boot when booting from QSPI? 0x40010000 or 0x40001000?
According to u-boot/README.qspi at integration · qoriq-open-source/u-boot · GitHub , it should be 0x1000 for LS1043A and we need to add the following PBI instruction to point to modify the boot location pointer:
write 0x570604, 0x40001000
However, ls1043aqds examples use 0x40010000 as boot location pointer. What is the correct offset?
As a follow-up question, is there an option to build a binary image for u-boot + rcw (not with SPL) with appropriate offsets using the LSDK or yocto toolchain?