ttyACM0 lost on ls1012ardb

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ttyACM0 lost on ls1012ardb

ソリューションへジャンプ
3,675件の閲覧回数
maumontadrien
Contributor III

Hi, after several tests on the ls1012ardb demo board, debug serial com ttyACM0 suddenly disappeared.

I can see the mass storage but no tty interface.

dmesg log:

[ 5609.803537] usb 1-1: new full-speed USB device number 14 using xhci_hcd
[ 5610.128702] usb 1-1: New USB device found, idVendor=0d28, idProduct=0204
[ 5610.128705] usb 1-1: New USB device strings: Mfr=1, Product=2, SerialNumber=3
[ 5610.128706] usb 1-1: Product: MBED CMSIS-DAP
[ 5610.128707] usb 1-1: Manufacturer: MBED
[ 5610.128708] usb 1-1: SerialNumber: 0201E76BF70B526D1306
[ 5610.129698] usb-storage 1-1:1.0: USB Mass Storage device detected
[ 5610.129911] scsi15 : usb-storage 1-1:1.0
[ 5611.137485] scsi 15:0:0:0: Direct-Access     MBED     microntroller    1.0  PQ: 0 ANSI: 2
[ 5611.138086] sd 15:0:0:0: Attached scsi generic sg4 type 0
[ 5611.140438] sd 15:0:0:0: [sdd] 1072 512-byte logical blocks: (548 kB/536 KiB)
[ 5611.142295] sd 15:0:0:0: [sdd] Write Protect is off
[ 5611.142300] sd 15:0:0:0: [sdd] Mode Sense: 03 00 00 00
[ 5611.143364] sd 15:0:0:0: [sdd] No Caching mode page found
[ 5611.143369] sd 15:0:0:0: [sdd] Assuming drive cache: write through
[ 5611.152350]  sdd:
[ 5611.155020] sd 15:0:0:0: [sdd] Attached SCSI removable disk

I tested this on different pc and on windows and linux with the same result.
タグ(2)
0 件の賞賛
返信
1 解決策
3,472件の閲覧回数
maumontadrien
Contributor III

I find the solution, I reprogram K20 debug mcu like it's explained in this Recovering Serial Connection on FRDM-LS1012A | Dzu's Blog .

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
3,473件の閲覧回数
maumontadrien
Contributor III

I find the solution, I reprogram K20 debug mcu like it's explained in this Recovering Serial Connection on FRDM-LS1012A | Dzu's Blog .

0 件の賞賛
返信
3,472件の閲覧回数
zmlopez
Contributor III

Don't forget to also disable Windows storage services, as is explained in this link:

DAPLink bootloader update | Mbed 

or the problem will happen again.

0 件の賞賛
返信
3,472件の閲覧回数
maumontadrien
Contributor III

Thank you for your help, I read serial on J24. I can read character at boot, but characters do not mean anything (I test in 115200/8/N/1 and with others speed.

I have the same problem on LS1012AFRDM board. I have an ls1021twr board which works fine.

Is there a solution to upgrade the K20 MCU ?

0 件の賞賛
返信
3,472件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello maumont adrien,

Please check switch setting SW1 [7](CFG_UART_MUX_EN_B).

0- LS1012A UART1 is connected to K22 UART0 for CMSIS DAP debug.

1 - LS1012A UART1 is translated to RS232 levels and is available on 1x3 header (J24).

Please configure SW1 [7] as 1 to use RS232 serial mode.


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信