strongswan

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

strongswan

2,212 Views
2979338158
Contributor I

Hello, when I use NXP openwrt ls1012a to execute strongswan IPSec to build a tunnel, the kernel will report the following errors. Thank you very much for your help in analyzing them.

Error messages are in the vicinity !

Labels (1)
0 Kudos
Reply
2 Replies

2,026 Views
bpe
NXP Employee
NXP Employee

Consider using NXP ASK which is based on OpenWRT customized and verified
on LS1012A-based boards:

Layerscape 1012A Broadband Home Router Application | NXP 

The ASK offers an NXP verified and HW-accelerated IPSec solution.

Regards,

Platon

0 Kudos
Reply

2,026 Views
bpe
NXP Employee
NXP Employee

Can you please mention the exact name and version of the NXP SDK/BSP you are
working with?

Best Regards,

Platon

0 Kudos
Reply