qorlq sdk problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

qorlq sdk problem

2,101件の閲覧回数
lingyunhui
Contributor I

When install the sdk,running "bitbake fsl-image-minimal",it occurs an error 'Failed to create SSTATE_DIR directory in which to run long name sanity check: Permission denied. You could try using /home/QorIQ-SDK-V1.7-20141218-yocto/poky/build_p1010rdb_release/../sstate-cache in SSTATE_MIRRORS rather than as an SSTATE_CACHE.'How to deal with it?Thank you.

0 件の賞賛
返信
1 返信

1,612件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Yunhui,


Please install both SOURCE ISO and CACHE ISO fro PPCE500V2, the Cache ISO contains build binaries to accelerate the building to avoid perform your build from the scratch.


The folder sstate-cache should be created when installing the Cache ISO.

In addition, please install ISOs with the normal user permission rather than root permission.

If your problem remains, please attach your build log.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信