mpc8572 toolchain

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

mpc8572 toolchain

1,295件の閲覧回数
andrewmotorin
Contributor I

I have reference board mpc8572ds with e500v2 cores as a target and x86_64 machine with ubuntu 16.04 as a host, and i want to compile some applications written in Ada language. To get started i've used powerpc-linux-gnu toolchain, but due to floating point issue this toolchain is not proper for that, so i've thought to change toolchain to powerpc-linux-gnuspe. The problem is that spe-toolchain from ubuntu repo is not support Ada. So, how could i get gcc spe-toolchain for my purpose?

0 件の賞賛
返信
1 返信

1,213件の閲覧回数
Pavel
NXP Employee
NXP Employee

Look at the following pages about LTIB toolchain:

http://ltib.org/documentation-LtibFaq

 

and

 

http://ltib.org/pages/LTIB_generic_v1.4_-_version_6.4.1.pdf

 

https://lists.nongnu.org/archive/html/ltib/2010-07/msg00172.html


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信