ls1024 clock specs

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

ls1024 clock specs

1,062 次查看
mipetouris
Contributor I

I want to know the amplitude range and the rise time for the 48MHz clock input of the LS1024

0 项奖励
回复
1 回复

1,017 次查看
alexander_yakov
NXP Employee
NXP Employee

48Mhz clock input (PS_XI) is a crystal input, it requires 3.3V sinusoidal input. Therefore, no slew rate is specified.


Have a great day,
Alexander,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复