ls1021/2 CAN bus issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ls1021/2 CAN bus issue

1,607 Views
liyingchun
Contributor I

Hi

ls1021/2 have 4 can bus controller.  I want to know that if the lsl02x cpu support wake up from can bus?

Tags (2)
0 Kudos
Reply
1 Reply

1,444 Views
lunminliang
NXP Employee
NXP Employee

Hello li yingchun,

According to the LS1021ARM, there are five basic mechanisms to wake up the chip from deep sleep:

• Ethernet event

• UART Activity

• I2C Bus Activity such as reception of packet.

• Internal timer event

• External pin event

So I am afraid no.

Have a great day,
Lunmin

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply