how do i get u-boot-with-spl-pbl.bin?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how do i get u-boot-with-spl-pbl.bin?

ソリューションへジャンプ
5,373件の閲覧回数
jayarajrajappan
Contributor II

How do i get u-boot-with-spl-pbl.bin?

QorIQ Processors

0 件の賞賛
返信
1 解決策
4,341件の閲覧回数
sinanakman
Senior Contributor III

Hi Jayaraj

I am not sure which SoC/board you are referring

to but as an example for LS1021xTWR board

here is how you can produce it using mainline

u-boot :

make distclean

make ls1021atwr_sdcard_defconfig

make all

with this you would have u-boot-with-spl-pbl.bin

generated and you could boot with this from SD.

Hope this helps

Sinan Akman

元の投稿で解決策を見る

3 返答(返信)
4,341件の閲覧回数
lunminliang
NXP Employee
NXP Employee

Hi,

Some supplement, this is also possible in SDK:

1. Change the config in /meta-fsl-arm/conf/machine/ls1021atwr.conf

    “ UBOOT_CONFIG ??= "sdcard"

2. $bitbake u-boot -c cleansstate

    $bitbake u-boot

Regards

Lunmin

0 件の賞賛
返信
4,342件の閲覧回数
sinanakman
Senior Contributor III

Hi Jayaraj

I am not sure which SoC/board you are referring

to but as an example for LS1021xTWR board

here is how you can produce it using mainline

u-boot :

make distclean

make ls1021atwr_sdcard_defconfig

make all

with this you would have u-boot-with-spl-pbl.bin

generated and you could boot with this from SD.

Hope this helps

Sinan Akman

4,341件の閲覧回数
jayarajrajappan
Contributor II

We are using LS1021A TWR board. We were able to build u-boot-with-spl-pbl.bin using the above steps and boot the card from SD. It helped us to reprogram the RCW on NOR bank 0 since we had accidentally erased it. Appreciate your help.

0 件の賞賛
返信