hi

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

hi

1,088 Views
hyun
Contributor I

P1010 processor ::   USB mouse  problem ::  USB disconnect

====

log === somtime   disconnect and connet

dvr login: usb 1-1.1: USB disconnect, device number 3

usb 1-1.1: new low speed USB device number 4 using fsl-ehci

input: PIXART USB OPTICAL MOUSE as /devices/soc.4/ffe22000.usb/fsl-ehci.0/usb1/1-1/1-1.1/1-1.1:1.0/input/input1

generic-usb 0003:093A:2510.0002: input: USB HID v1.11 Mouse [PIXART USB OPTICAL MOUSE] on usb-fsl-ehci.0-1.1/input0

usb 1-1.1: USB disconnect, device number 4

usb 1-1.1: new low speed USB device number 5 using fsl-ehci

input: PIXART USB OPTICAL MOUSE as /devices/soc.4/ffe22000.usb/fsl-ehci.0/usb1/1-1/1-1.1/1-1.1:1.0/input/input2

generic-usb 0003:093A:2510.0003: input: USB HID v1.11 Mouse [PIXART USB OPTICAL MOUSE] on usb-fsl-ehci.0-1.1/input0

usb 1-1.1: USB disconnect, device number 5

usb 1-1.1: new low speed USB device number 6 using fsl-ehci

input: PIXART USB OPTICAL MOUSE as /devices/soc.4/ffe22000.usb/fsl-ehci.0/usb1/1-1/1-1.1/1-1.1:1.0/input/input3

generic-usb 0003:093A:2510.0004: input: USB HID v1.11 Mouse [PIXART USB OPTICAL MOUSE] on usb-fsl-ehci.0-1.1/input0


Original Attachment has been moved to: usb-err1.txt.zip

0 Kudos
Reply
0 Replies