fsl_lpuart driver api

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

fsl_lpuart driver api

3,495 Views
ser_fr
Contributor I

Hello, I try to init lpuart on ls1020a custom board using fsl_lpuart linux kernel driver. Where I can find fsl_lpuart driver api reference manual and what's the procedure of initialization lpuart?

Tags (1)
0 Kudos
Reply
4 Replies

3,362 Views
Pavel
NXP Employee
NXP Employee

Linux driver for LPUART provides creation new TTY.

See the following pages about using LPUART TTY:

https://developer.toradex.com/knowledge-base/uart-(linux)

 

https://lore.kernel.org/patchwork/patch/994736/

Have a great day,
Pavel Chubakov

0 Kudos
Reply

3,362 Views
ser_fr
Contributor I

Thanks, Pavel, will be study the information. пятница, 01 ноября 2019г., 07:56 +03:00 от Pavel [email protected] :

>NXP Community

>Re: fsl_lpuart driver api

>reply from Pavel Chubakov in QorIQ Processing Platforms - View the full discussion

0 Kudos
Reply

3,362 Views
Pavel
NXP Employee
NXP Employee

See the Section 7.10.1 from SDK 2.0-1703 documentation about LPUART using:

https://www.nxp.com/docs/en/supporting-information/QORIQ-SDK-2.0-IC-REV0.pdf

Have a great day,
Pavel Chubakov

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

3,362 Views
ser_fr
Contributor I

Hello, Pavel!

This Section contains information only about location of the LPUART driver source file "drivers/tty/serial/fsl_lpuart.c". l interest how to work with this driver? What's the procedure of init and configuration lpuart port from custom application? Now I use "termios.h" api and have a difficulties with configuration max possible baud rate and edma rx use.

Thanks четверг, 31 октября 2019г., 08:28 +03:00 от Pavel [email protected] :

>NXP Community

>Re: fsl_lpuart driver api

>reply from Pavel Chubakov in QorIQ Processing Platforms - View the full discussion

0 Kudos
Reply