Hi,
I'm using yocto SDK 2.0, In which i'm trying to build Linux image for T4240RDB.
Following is the procedure followed:
1. bitbake -c menuconfig virtual/kernel
2. bitbake -c compile -f virtual/kernel
3. bitbake virtual/kernel
4. bitbake fsl-image-kernelitb
When i give "bitbake fsl-image-kernelitb",
"ERROR: Nothing PROVIDES 'fsl-image-kernelitb'
ERROR: fsl-image-kernelitb was skipped: incompatible with machine t4240rdb-64b (not in COMPATIBLE_MACHINE)" is displayed.
Could you please help me to proceed further.
Waiting for your reply..!
Thanks & Regards,
Mounika Reddy
The T4240 u-boot does not supports .itb files. There is no the fsl-image-kernelitb.bbappend for the T4240.
Have a great day,
Pavel Chubakov
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
NXP SDK 2.0 does not support kernelitb for the T4240. This option is available for the LS1012a. LS1043a and LS1046a. See the following file:
QorIQ-SDK-V2.0-20160527-yocto/sources/meta-nxp-npi-1703/recipes-fsl/images/fsl-image-kernelitb.bbappend
Have a great day,
Pavel Chubakov
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi,
Thank you for the reply..!
I have few more doubts:
1. Were I can download the fsl-image-kernelitb.bbappend ?
2. If I download and add the fsl-image-kernelitb.bbappend file to recipe folder will it work straight away or I need to do any changes?
Could you please suggest me the procedure?
Thanks & Regards,
Mounika Anugula
Design Engineer
Mobile : (+91) 9916711639
Website : <http://www.coreel.com> www.coreel.com
Ph: (+91)80-41970400
Fax: (+91)80-30723638
CoreEL Technologies,
#21, 7th Main, 1st Block , Koramangala,
Bangalore 560034
<https://www.facebook.com/CoreELTechnologies> Description: Description: Image result for facebook icon in orange <https://www.linkedin.com/company/coreel-technologies?trk=company_logo> Description: Description: Image result for facebook icon in orange
Description: COREEL~1 - Copy.JPG