flexbuild_lsdk2108 Building CST error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

flexbuild_lsdk2108 Building CST error

1,793件の閲覧回数
hongyuanz
Contributor IV

Building CST ...
not found valid repo info for cst
make[3]: *** [/flexbuild/packages/apps/security/cst.mk:10: cst] Error 1
make[3]: Leaving directory '/flexbuild/packages/apps'
make[2]: *** [Makefile:25: cst] Error 2
make[2]: Leaving directory '/flexbuild'
cp: cannot stat '/flexbuild/components/apps/security/cst/srk.*': No such file or directory
BL32=NULL as OPTEE is not enabled
make -s -j32 fip pbl PLAT=ls1046apscb BOOT_MODE=sd RCW=firmware/rcw/ls1046apscb/NN_FNSNPPPP_1133_8888/rcw_1600_sdboot_sben.bin BL33=/flexbuild/build/firmware/u-boot/ls1046apscb/uboot_ls1046apscb_tfa_SECURE_BOOT.bin TRUSTED_BOARD_BOOT=1 CST_DIR=/flexbuild/components/apps/security/cst
make[2]: Entering directory '/flexbuild/components/firmware/atf'
board PAth = plat/nxp/soc-ls1046a/ls1046apscb
setting chssis
SFP in BL2 code
Generating CSF Header for /flexbuild/components/firmware/atf/build/ls1046apscb/release/bl33.bin.cst /flexbuild/build/firmware/u-boot/ls1046apscb/uboot_ls1046apscb_tfa_SECURE_BOOT.bin

make[2]: /flexbuild/components/apps/security/cst/create_hdr_esbc: Command not found
make[2]: *** [Makefile:1128: /flexbuild/components/firmware/atf/build/ls1046apscb/release/bl33.bin.cst] Error 127
make[2]: *** Waiting for unfinished jobs....
Building tools/fiptool/fiptool
HOSTCC fiptool.c
HOSTCC tbbr_config.c
HOSTLD fiptool

Built fiptool successfully


make[2]: Leaving directory '/flexbuild/components/firmware/atf'
cp: cannot stat 'build/ls1046apscb/release/bl2_sd*.pbl': No such file or directory
make[1]: *** [atf.mk:11: atf] Error 1
make[1]: Leaving directory '/flexbuild/packages/firmware'
make: *** [Makefile:19: atf] Error 2
make: Leaving directory '/flexbuild'

 

0 件の賞賛
返信
1 返信

1,558件の閲覧回数
cmx
Contributor I

This happened to me after doing a bld clean-firmware.

Tried a full build (i.e. bld -m ls1028ardb) and re-fetching al the repos; ultimately had to delete my flexbuild environment and start over.

0 件の賞賛
返信