ethtool support in mpc8250

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ethtool support in mpc8250

1,931件の閲覧回数
saurabhagarwal
Contributor III

I have mpc8250 based embedded system that has kernel version 2.6.24. I want to use ethtool or mii-tool in this system. I cross compiled ethtool package for powerpc mpc8250 cpu.

when i use ethtool, I get following error

 ./ethtool -i eth0 Cannot get driver information: Operation not supported 

with mii-tool, I get following error

 ./mii-tool SIOCGMIIPHY on 'eth0' failed: Operation not supported 

Is ethtool or mii-tool suppoerted on mpc8250 ?

タグ(2)
0 件の賞賛
返信
1 返信

1,597件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

If I understand the question properly, the question is more related to ethernet driver you are using than to MPC8250 hardware.

According to Linux kernel version you specified, this does not seem to be Freescale Linux BSP we offer for this MPC8250 device.

Please address this question to your Linux vendor.

0 件の賞賛
返信