ethtool support in mpc8250

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ethtool support in mpc8250

1,926 Views
saurabhagarwal
Contributor III

I have mpc8250 based embedded system that has kernel version 2.6.24. I want to use ethtool or mii-tool in this system. I cross compiled ethtool package for powerpc mpc8250 cpu.

when i use ethtool, I get following error

 ./ethtool -i eth0 Cannot get driver information: Operation not supported 

with mii-tool, I get following error

 ./mii-tool SIOCGMIIPHY on 'eth0' failed: Operation not supported 

Is ethtool or mii-tool suppoerted on mpc8250 ?

Tags (2)
0 Kudos
Reply
1 Reply

1,592 Views
alexander_yakov
NXP Employee
NXP Employee

If I understand the question properly, the question is more related to ethernet driver you are using than to MPC8250 hardware.

According to Linux kernel version you specified, this does not seem to be Freescale Linux BSP we offer for this MPC8250 device.

Please address this question to your Linux vendor.

0 Kudos
Reply