dsp boot source code B4860

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

dsp boot source code B4860

Jump to solution
5,929 Views
Marklyu
Contributor I

i use the QorIQ-SDK-1_7-IC-RevA, 

i see the chapter 8 linux user space  IPC, there is dsp_boot (source code of dsp boot loader)part. want to know where can i get/download the source code of it ? the dsp_boot source code is included in the sdk which folder ?

 

Regards,

Mark

0 Kudos
Reply
1 Solution
5,897 Views
yipingwang
NXP TechSupport
NXP TechSupport

In your Yocto build environment, please run the following command.

$ bitbake ipc-ust -c patch -f

You will get dsp_boot source code in folder.

build_b4860qds/tmp/work/ppce6500-fsl-linux/ipc-ust/git-r0/git/dsp_boot/

View solution in original post

0 Kudos
Reply
9 Replies
5,898 Views
yipingwang
NXP TechSupport
NXP TechSupport

In your Yocto build environment, please run the following command.

$ bitbake ipc-ust -c patch -f

You will get dsp_boot source code in folder.

build_b4860qds/tmp/work/ppce6500-fsl-linux/ipc-ust/git-r0/git/dsp_boot/

0 Kudos
Reply
5,844 Views
Marklyu
Contributor I

i follow your advice , and the log as below. then there is no source code folder.

build_b4860qds-64b_release]$ bitbake ipc-ust -c patch -f
WARNING: Host distribution "CentOS-7.2.1511" has not been validated with this version of the build system; you may possibly experience unexpected failures. It is recommended that you use a tested distribution.
Loading cache: 100% |######################################| ETA: 00:00:00
Loaded 3921 entries from dependency cache.
NOTE: Resolving any missing task queue dependencies

Build Configuration:
BB_VERSION = "1.22.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "CentOS-7.2.1511"
TARGET_SYS = "powerpc64-fsl-linux"
MACHINE = "b4860qds-64b"
DISTRO = "fsl-networking"
DISTRO_VERSION = "1.6"
TUNE_FEATURES = "m64 fpu-hard e6500 altivec"
TARGET_FPU = "hard"
meta
meta-yocto
meta-yocto-bsp = "(detachedfromfsl-sdk-v1.6):0d2ce44c2b0f8cc9699e30cca2c24655be89d58b"
meta-fsl-ppc = "(detachedfromfsl-sdk-v1.6):6cf59d9de63a9fc5f8942c0d10c622898f4315ce"
meta-fsl-ppc-toolchain = "(detachedfromfsl-sdk-v1.6):a546e42f86e7d57de19e27907365d170b13fc18f"
meta-fsl-networking
meta-fsl-networking = "(detachedfrom8dec9c6):8dec9c690188cce5305ef5055f91e5cfa35c63f4"
meta-virtualization
meta-virtualization = "(detachedfromfsl-sdk-v1.6):8044073f63a0d99541a43ac5f2f6d789f94c7c7c"
meta-oe
meta-networking
meta-webserver
meta-ruby
meta-filesystems = "(detachedfromfsl-sdk-v1.6):b86007f742a1b829ccc8d76e485bb3f789cefaa4"
meta-java = "(detachedfromfsl-sdk-v1.6):d01f7d39e513790ddce20e6724723722119a3700"
meta-openstack
meta-openstack-compute-deploy
meta-openstack-controller-deploy
meta-openstack-qemu = "(detachedfromfsl-sdk-v1.6):f627404399a134672e0b5e26a0d9b794a6f8adf4"

NOTE: Preparing runqueue
NOTE: Tainting hash to force rebuild of task /sdb/marklyu/QorIQ-SDK-V1.6-20140619-yocto/meta-fsl-ppc/recipes-bsp/ipc/ipc-ust_git.bb, do_patch
NOTE: Executing SetScene Tasks
NOTE: Executing RunQueue Tasks
NOTE: Tasks Summary: Attempted 10 tasks of which 9 didn't need to be rerun and all succeeded.

Summary: There was 1 WARNING message shown.

0 Kudos
Reply
5,841 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please check whether build_b4860qds/tmp/work/ppce6500-fsl-linux/ipc-ust exists.

0 Kudos
Reply
5,836 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please go to folder build_b4860qds/tmp/work/ and run the following command.

find . -name ipc-ust

0 Kudos
Reply
5,816 Views
Marklyu
Contributor I

thanks much . found the source code files at ppc64e6500-fsl-linux/ipc-ust/git-r0/git.

0 Kudos
Reply
5,814 Views
yipingwang
NXP TechSupport
NXP TechSupport

OK, thanks.

0 Kudos
Reply
5,838 Views
Marklyu
Contributor I

no, there is no ipc-ust folder under the  ppce6500-fsl-linux.

 

ppce6500-fsl-linux]$ ls
lib32-binutils lib32-gettext lib32-ncurses
lib32-binutils-cross lib32-gmp lib32-openssl
lib32-bison lib32-inputproto lib32-opkg-utils
lib32-bzip2 lib32-kbproto lib32-perl
lib32-cryptodev-headers lib32-libgcc lib32-python
lib32-db lib32-libmpc lib32-readline
lib32-eglibc lib32-libpthread-stubs lib32-sqlite3
lib32-eglibc-initial lib32-libtool-cross lib32-util-macros
lib32-expat lib32-libx11 lib32-valgrind
lib32-flex lib32-libxau lib32-xcb-proto
lib32-gcc lib32-libxcb lib32-xextproto
lib32-gcc-cross lib32-libxdmcp lib32-xproto
lib32-gcc-cross-initial lib32-linux-libc-headers lib32-xtrans
lib32-gcc-runtime lib32-m4 lib32-zlib
lib32-gdbm lib32-mpfr

0 Kudos
Reply
5,893 Views
Marklyu
Contributor I
thanks much for your answer!!!
0 Kudos
Reply
5,892 Views
yipingwang
NXP TechSupport
NXP TechSupport

Welcome

0 Kudos
Reply