Windows driver

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Windows driver

1,242 Views
sivaramanradhak
Contributor I

Hi NXP,

Can communication processors from QorIQ supports 802.11 a/b/g/n/ac chips with windows drivers?

Please let us know any Windows driver supporting communication processor and wifi module.

Thanks,

Siva

0 Kudos
Reply
1 Reply

1,187 Views
alexander_yakov
NXP Employee
NXP Employee

Windows driver is typically used to run hardware on Windows OS. As per information we currently have, for this particular moment there is Windows OS does not support QorIQ platform, and OS vendor does not have plans to support this platform.

There is a number of other Operating Systems on the market supporting our QorIQ processors. Please specify, which particular operating system your question is about. If this OS is proprietary, than please address your question to OS vendor. If your OS is Linux, than you need Linux driver to support your 802.11 a/b/g/n/ac chip. Typically, driver is offered by chip vendor, so please contact chip vendor with question is they offer drivers for Linux. We do not have experience running 802.11 a/b/g/n/ac chip in Linux with drivers from Windows, this is not usual case.


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply