What is specific CPU Frequency of the processor on P2020RDB: P2020 Reference Design Board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What is specific CPU Frequency of the processor on P2020RDB: P2020 Reference Design Board

795件の閲覧回数
sagee
Contributor I

I'm considering purchasing the P2020RDB but I can not seem to find any information on which P2020 is being used.  I need to find the CPU speed of the processor used.

0 件の賞賛
返信
1 返信

717件の閲覧回数
r8070z
NXP Employee
NXP Employee


Have a great day,

Typically the P2020RDB has P2020 QorIQ 1200MHZ 1.05V TEPBGA689. The P2020RDB-PCA Quick Start Guide says:

“Key Features of the P2020RDB-PCA 

  Freescale QorIQ architecture CPU

   QorIQ P2020E, 1200 MHz "

I expect that P2020NSE2MHC is installed on the currently available P2020RDB-PCA board. However you may ask the board distributor for confirmation.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信