TLB and MMu

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TLB and MMu

1,318 Views
monalihaware
Contributor III

In the init files of qor iq(t series), tlbs are progrmed.

1.  What Are the CAM registers and where are they located? In t2080, in e6500 manual  I am not abke to find them.

2. Is it necessary to program tlbs in the bare board while bribginb it up? Without the tlbs , cant I access and write directly into LAWs and IFC, DDR registers and access flash and DDr memories??

3.are the addresses which we program in the init files the effective addresses or physical addresses of peripherals like e8000000 for flash etc.

Tags (2)
0 Kudos
Reply
1 Reply

1,227 Views
ufedor
NXP Employee
NXP Employee

1) The CAM registers are described in the CodeWarrior Development Studio for Power Architecture Processors Targeting Manual, 5.10.5.4.5 e6500 Registers.

2) It is required to initialize TLBs for accessing CCSR, IFC banks and DDR SDRAM area.

3) Physical.

0 Kudos
Reply