T2081 PCIe problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

T2081 PCIe problem

5,012件の閲覧回数
gyosunshim
Contributor III

Hi All,

 

I am using the T2081 board made.

PCIex4 lanes of the T2081 has confirmed that the recognition by connecting to Altera FPGA.

 

* boot log

...

PCIe4: Root Complex, x4 gen1, regs @ 0xfe270000

  01:00.0     - 1172:0004 - Does not fit any class

......

PCI host bridge /pcie@ffe270000  ranges:

MEM 0x0000000c40000000..0x0000000c4fffffff -> 0x00000000e0000000

  IO 0x0000000ff8030000..0x0000000ff803ffff -> 0x0000000000000000

 

# lspci

00:00.0 Class 0604: 1957:0839

01:00.0 Class ff00: 1172:0004 <-- Altera FPGA

 

# cat /proc/iomem

00000000-ffffffff : System RAM

c40000000-c4fffffff : /pcie@ffe270000

  c40000000-c4fffffff : PCI Bus 0000:01

    c40000000-c400003ff : 0000:01:00.0

    c40000400-c400007ff : 0000:01:00.0

    c40000800-c40000bff : 0000:01:00.0

fe8000000-fefffffff : fe8000000.nor

........

 

Use the mmap64 receive an error as shown in Table 1, we read the 0xc40000000 address.

Table 1

Machine check in kernel mode.

Caused by (from MCSR=a000): Load Error Report

Guarded Load Error Report

Oops: Machine check, sig: 7 [#1]

SMP NR_CPUS=24 CoreNet Generic

Modules linked in:

CPU: 0 PID: 1719 Comm: console_mmap Not tainted 3.12.37-rt51-QorIQ-SDK-V1.8+gf488de6 #7

task: c0000000e069d540 ti: c0000000e0e00000 task.ti: c0000000e0e00000

NIP: 0000000010000f88 LR: 0000000010000f58 CTR: c000000000306128

REGS: c0000000e0e03ea0 TRAP: 0000   Not tainted  (3.12.37-rt51-QorIQ-SDK-V1.8+gf488de6)

MSR: 000000000002f000 <CE,EE,PR,FP,ME>  CR: 28000288  XER: 20000000

SOFTE: 1

 

 

GPR00: 0000000010000f58 00000000ffc7d2c0 00000000f7e7a4c0 0000000000000025

GPR04: 000000000fee0544 0000000000000000 0000000000004000 0000000010002185

GPR08: 0000000000000000 00000000f7e72000 00000000f7e72000 00000000ffc7d230

GPR12: 0000000044000222 000000001001a570 00000000100f0000 0000000000000000

GPR16: 0000000000000000 00000000100f46cc 00000000100f46bc 00000000100f0000

GPR20: 00000000100f48d8 0000000044444444 0000000000000000 000000001010f508

GPR24: 0000000000000000 000000001010f448 0000000000000000 00000000f7e76f18

GPR28: 00000000f7e77840 0000000000000000 000000000ffed344 00000000ffc7d2c0

NIP [0000000010000f88] 0x10000f88

LR [0000000010000f58] 0x10000f58

Call Trace:

---[ end trace 83d2ce4957171a6e ]---

 

 

[READ 10 BYTE DATA from 0x00000000]

Bus error

 

What's the problem?

If I may be so FPGA logic problem?

Attach the boot log.

 

Thank you.

Best regards,

gyosun.

Original Attachment has been moved to: t2081_boot.log.zip

0 件の賞賛
返信
6 返答(返信)

3,486件の閲覧回数
evaneimer
Contributor I

I was getting a similar error when trying to write to a device in the PCIe window (read worked fine, but writes caused a crash).  Turns out it was a programming error on my part.  I was using the following, which was wrong:

int fd = open("/dev/mem", O_SYNC);
fpgaAddr = mmap(NULL, 0x100000, PROT_READ | PROT_WRITE, MAP_PRIVATE, fd, 0xc40000000);

When I corrected to this, everything worked fine:

int fd = open("/dev/mem", O_SYNC|O_RDWR);
fpgaAddr = mmap(NULL, 0x100000, PROT_READ | PROT_WRITE, MAP_SHARED, fd, 0xc40000000);

0 件の賞賛
返信

3,486件の閲覧回数
bpe
NXP Employee
NXP Employee

Machine check interrupt occurs (among other reasons) when the transaction

target does not respond. This may occur both because the target address

is invalid and because the target is not responding. Based on the

information in this post, it is not possible to determine what exactly

happens. The suggestions are:

1. Connect a good JTAG debugger to the system.

2. Step through your code, verify  the parameters you pass to

   mmap() and related calls. Make sure your code checks for errors

   returned by mmap() befor using the pointer.

  

3. Try your code with a PCIe peripheral that is known working.  

  

4. For hardware-level errors, immediately after machine check inspect registers

   discussed in    Sections 8.3.1.3 and 20.6.1.12 of the chip Reference Manual.  


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

3,484件の閲覧回数
tiagobrusamarel
Contributor V

Hello bpe.

I'm having the same issue that gyosun is having. I'm getting the Machine Check exception when trying to read from PCIe4 I/O address space.

We have 2 custom CPU boards with QorIQ processors: one with the T2081 and another with the T1022. For the application we have a custom base board with the PCIe (x1 Gen2) link partner connected to SerDes lane E.

When using the T1022 CPU board I can communicate with the link partner normally. But with the T2081 I'm getting the Machine Check exception all the time.

The kernel driver for that is basically the same, with the difference that the T1022 runs in 32 bit mode and the T2081 in 64bit mode.

Please find attached the register's dump generated from the Corewarrior Debugger at the moment of the failure.

Could you please help me find out whats is wrong?

Thanks,

Tiago.

0 件の賞賛
返信

3,484件の閲覧回数
tiagobrusamarel
Contributor V

Hello again.

I found out what was the cause of my problems with PCIe4: I was using wrong memory ranges for PCIe device nodes on our board DTS file. After copying the memory ranges defined for the T2080RDB board the problem was solved.

Regards,

0 件の賞賛
返信

3,484件の閲覧回数
gyosunshim
Contributor III

Hello Tiago,

Be glad to solve the problem. I 's still a problem.

What, and Where is the DTS?

How can you explain in detail that you solve the problem?

PCIe is connected to four lanes, as shown below.

pcie connection.png

Thanks,

Gyosun.

0 件の賞賛
返信

3,484件の閲覧回数
gyosunshim
Contributor III

Hi bpe,

Thank you for answer.

Current structural JTAG hardware is unable to connect. No JTAG port.

CCSR register is well below the code. When you access the PCIE error.

int fd;

uint8_t *vaddr;

uint64_t baddr = 0xc40000000; // PCIe BAR0

//uint64_t baddr = 0xffe000000; // CCSR

fd = open("/dev/mem", O_RDWR | O_SYNC);

vaddr = (uint8_t *)mmap64(NULL, 0x400, PROT_READ | PROT_WRITE, MAP_SHARED, fd, baddr);

printf("%08x\r\n", *(uint32_t *)(vaddr));

close(fd);

When added to the PCIE no logic in the FPGA and stopped by reading the PCIE Register, when the PCIE logic is a kernel error message is output.

If you have any problems logic FPGA PCIE possible error occurs when using mmap?

I'm not sure what the problem. We need more help.

Best regards,

gyosun.

0 件の賞賛
返信