T2080 Secure Boot : Enqueuing to SEC error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T2080 Secure Boot : Enqueuing to SEC error

20 Views
ganesh_sullad
Contributor I

Hi,

We are seeing 0x700 in the scratch register SCRATCHRW2, which corresponds to ERROR_SEC_ENQ as per Trust 2.0 device ISBC error codes. 

What are the possible reasons this error will show up? Could you guide on this?

Few other details: 

Using custom image, generated RSA key pairs using CST, generated CSF, digital signature and loaded on the T2080RDB setup. Upon code execution the above observation was made. 

OTPMK is fused, no error observed on the Security Monitor registers. 

SRKH is updated through script(using debugger) with values given by CST tool. 

Let me know if additional details are necessary. 

Note: If require, i can share the NDA file number. 

 

Tags (1)
0 Kudos
Reply
0 Replies