T2080:Qman ErrInt: Corenet Initiator Data Error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

T2080:Qman ErrInt: Corenet Initiator Data Error

3,248件の閲覧回数
qwertyuiop
Contributor I

Here are my kernel initialization info.Kernel will not work when the error appeared.

Hope can find some help

Best regard.

WARNING: adjusting available memory to 30000000
## Booting kernel from Legacy Image at 30000000 ...
Image Name: Linux-4.1.8-rt8+gbd51baf
Image Type: PowerPC Linux Kernel Image (gzip compressed)
Data Size: 5100608 Bytes = 4.9 MiB
Load Address: 00000000
Entry Point: 00000000
Verifying Checksum ... OK
## Flattened Device Tree blob at e8800000
Booting using the fdt blob at 0xe8800000
Uncompressing Kernel Image ... OK
Loading Device Tree to 03fe3000, end 03fff7c7 ... OK
Reserved memory: initialized node bman-fbpr, compatible id fsl,bman-fbpr
Reserved memory: initialized node qman-fqd, compatible id fsl,qman-fqd
Reserved memory: initialized node qman-pfdr, compatible id fsl,qman-pfdr
Reserved memory: initialized node pme-pdsr, compatible id fsl,pme-pdsr
Reserved memory: initialized node pme-sre, compatible id fsl,pme-sre
Reserved memory: initialized node usdpaa_mem, compatible id fsl,usdpaa-mem
Using CoreNet Generic machine description
MMU: Supported page sizes
4 KB as direct
2048 KB as direct & indirect
4096 KB as direct
16384 KB as direct
65536 KB as direct
262144 KB as direct
1048576 KB as direct
MMU: Book3E HW tablewalk enabled
bootconsole [udbg0] enabled
CPU maps initialized for 2 threads per core
Starting Linux PPC64 #1 SMP Tue Nov 1 11:47:15 CST 2016
-----------------------------------------------------
ppc64_pft_size = 0x0
phys_mem_size = 0x2000000
dcache_line_size = 0x40
icache_line_size = 0x40
cpu_features = 0x00180480581802c8
possible = 0x00180480581802c8
always = 0x00180400581802c0
cpu_user_features = 0xdc008000 0x08000000
mmu_features = 0x000a0010
firmware_features = 0x0000000000000000
-----------------------------------------------------
<- setup_system()
Linux version 4.1.8-rt8+gbd51baf (any888@any888) (gcc version 4.9.2 (GCC) ) #1 SMP Tue Nov 1 11:47:15 CST 2016
CoreNet Generic board
Zone ranges:
DMA [mem 0x0000000000000000-0x0000000001ffffff]
DMA32 empty
Normal empty
Movable zone start for each node
Early memory node ranges
node 0: [mem 0x0000000000000000-0x0000000001ffffff]
Initmem setup node 0 [mem 0x0000000000000000-0x0000000001ffffff]
MMU: Allocated 2112 bytes of context maps for 255 contexts
PERCPU: Embedded 17 pages/cpu @c000000001d00000 s28824 r0 d40808 u131072
Built 1 zonelists in Zone order, mobility grouping off. Total pages: 8080
Kernel command line: mem=32M console=ttyS0,115200 noinitrd root=/dev/mtdblock3 rw rootfstype=jffs2 init=/linuxrc
log_buf_len individual max cpu contribution: 4096 bytes
log_buf_len total cpu_extra contributions: 28672 bytes
log_buf_len min size: 16384 bytes
log_buf_len: 65536 bytes
early log buf free: 12144(74%)
PID hash table entries: 128 (order: -2, 1024 bytes)
Dentry cache hash table entries: 4096 (order: 3, 32768 bytes)
Inode-cache hash table entries: 2048 (order: 2, 16384 bytes)
Sorting __ex_table...
Cannot allocate SWIOTLB buffer
Memory: 17372K/32768K available (7856K kernel code, 1132K rwdata, 3008K rodata, 364K init, 764K bss, 15396K reserved, 0K cma-reserved)
Hierarchical RCU implementation.
RCU debugfs-based tracing is enabled.
CONFIG_RCU_FANOUT set to non-default value of 32
Additional per-CPU info printed with stalls.
RCU restricting CPUs from NR_CPUS=24 to nr_cpu_ids=8.
RCU: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=8
NR_IRQS:512 nr_irqs:512 16
mpic: Setting up MPIC " OpenPIC " version 1.2 at ffe040000, max 8 CPUs
mpic: ISU size: 512, shift: 9, mask: 1ff
mpic: Initializing for 512 sources
clocksource timebase: mask: 0xffffffffffffffff max_cycles: 0x8a5d528ca, max_idle_ns: 440795203517 ns
clocksource: timebase mult[1aab5972] shift[24] registered
Console: colour dummy device 80x25
pid_max: default: 32768 minimum: 301
Mount-cache hash table entries: 512 (order: 0, 4096 bytes)
Mountpoint-cache hash table entries: 512 (order: 0, 4096 bytes)
e6500 family performance monitor hardware support registered
Brought up 8 CPUs
devtmpfs: initialized
clocksource jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
xor: measuring software checksum speed
8regs : 3083.000 MB/sec
8regs_prefetch: 2732.000 MB/sec
32regs : 2591.000 MB/sec
32regs_prefetch: 2285.000 MB/sec
altivec : 4934.000 MB/sec
xor: using function: altivec (4934.000 MB/sec)
NET: Registered protocol family 16
Bman ver:0a02,02,01
qman-fqd addr 0xfffffe800000 size 0x800000
qman-pfdr addr 0xfffffc000000 size 0x2000000
Qman ver:0a01,03,01,02
Can't find hose for PCI bus 0!
EDAC PCI0: Giving out device to module MPC85xx_edac controller mpc85xx_pci_err: DEV ffe240000.pcie (INTERRUPT)
MPC85xx_edac acquired irq 20 for PCI Err
MPC85xx_edac PCI err registered
platform ffe240000.pcie:pcie@0: Invalid size 0xfffff9 for dma-range
Found FSL PCI host bridge at 0x0000000ffe270000. Firmware bus number: 0->1
PCI host bridge /pcie@ffe270000 ranges:
MEM 0x0000000c40000000..0x0000000c4fffffff -> 0x00000000e0000000
IO 0x0000000ff8030000..0x0000000ff803ffff -> 0x0000000000000000
/pcie@ffe270000: PCICSRBAR @ 0xff000007
setup_pci_atmu: end of DRAM 2000000
EDAC PCI1: Giving out device to module MPC85xx_edac controller mpc85xx_pci_err: DEV ffe270000.pcie (INTERRUPT)
MPC85xx_edac acquired irq 23 for PCI Err
MPC85xx_edac PCI err registered
platform ffe270000.pcie:pcie@0: Invalid size 0xfffff9 for dma-range
PCI: Probing PCI hardware
fsl-pci ffe270000.pcie: PCI host bridge to bus 0001:00
pci_bus 0001:00: root bus resource [io 0x10000-0x1ffff] (bus address [0x0000-0xffff])
pci_bus 0001:00: root bus resource [mem 0xc40000000-0xc4fffffff] (bus address [0xe0000000-0xefffffff])
pci_bus 0001:00: root bus resource [bus 00-01]
pci 0001:00:00.0: [Firmware Bug]: reg 0x10: invalid BAR (can't size)
pci 0001:00:00.0: PCI bridge to [bus 01-ff]
PCI: Cannot allocate resource region 6 of device 0001:00:00.0, will remap
pci 0001:00:00.0: BAR 6: no space for [mem size 0x01000000 pref]
pci 0001:00:00.0: BAR 6: failed to assign [mem size 0x01000000 pref]
pci 0001:00:00.0: PCI bridge to [bus 01]
pci 0001:00:00.0: bridge window [io 0x10000-0x1ffff]
pci 0001:00:00.0: bridge window [mem 0xc40000000-0xc4fffffff]
raid6: altivecx1 gen() 946 MB/s
raid6: altivecx2 gen() 1577 MB/s
raid6: altivecx4 gen() 2597 MB/s
raid6: altivecx8 gen() 2530 MB/s
raid6: int64x1 gen() 442 MB/s
raid6: int64x1 xor() 660 MB/s
raid6: int64x2 gen() 743 MB/s
raid6: int64x2 xor() 789 MB/s
raid6: int64x4 gen() 1137 MB/s
raid6: int64x4 xor() 873 MB/s
raid6: int64x8 gen() 978 MB/s
raid6: int64x8 xor() 708 MB/s
raid6: using algorithm altivecx4 gen() 2597 MB/s
raid6: using intx1 recovery algorithm
vgaarb: loaded
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
pps_core: LinuxPPS API ver. 1 registered
pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <[email protected]>
PTP clock support registered
EDAC MC: Ver: 3.0.0
bman-fbpr addr 0xffffff000000 size 0x1000000
fsl-pamu: pamu_av_isr: access violation interrupt
fsl-pamu: pamu_av_isr: POES1=00000000
fsl-pamu: pamu_av_isr: POES2=00000000
fsl-pamu: pamu_av_isr: AVS1=003f0081
fsl-pamu: pamu_av_isr: AVS2=00000081
fsl-pamu: pamu_av_isr: AVA=000000ffff000000
fsl-pamu: pamu_av_isr: UDAD=00000000
fsl-pamu: pamu_av_isr: POEA=0000000000000000
fsl-pamu: pamu_av_isr: Disabling liodn 3f
fsl-pamu: pamu_av_isr: access violation interrupt
fsl-pamu: pamu_av_isr: POES1=00000000
fsl-pamu: pamu_av_isr: POES2=00000000
fsl-pamu: pamu_av_isr: AVS1=003f0081
fsl-pamu: pamu_av_isr: AVS2=00000081
fsl-pamu: pamu_av_isr: AVA=000000ffff060000
fsl-pamu: pamu_av_isr: UDAD=00000000
fsl-pamu: pamu_av_isr: POEA=0000000000000000
Bman err interrupt handler present
Bman portal initialised, cpu 0
Bman portal initialised, cpu 1
Bman portal initialised, cpu 2
Bman portal initialised, cpu 3
Bman portal initialised, cpu 4
Bman portal initialised, cpu 5
Bman portal initialised, cpu 6
Bman portal initialised, cpu 7
Bman portals initialised
Qman err interrupt handler present
QMan: Allocated lookup table at 8000000000002000, entry count 131073
Qman portal initialised, cpu 0
Qman portal initialised, cpu 1
Qman portal initialised, cpu 2
Qman portal initialised, cpu 3
Qman portal initialised, cpu 4
Qman portal initialised, cpu 5
Qman portal initialised, cpu 6
Qman portal initialised, cpu 7
Qman portals initialised
Bman: BPID allocator includes range 32:32
Qman: FQID allocator includes range 256:512
Qman: FQID allocator includes range 32768:32768
Qman: CGRID allocator includes range 0:256
Qman: pool channel allocator includes range 1025:15
USDPAA region at ffffe0000000:10000000(ffffe0000:10000), 1 TLB1 entries)
fsl-ifc ffe124000.localbus: Freescale Integrated Flash Controller
fsl-ifc ffe124000.localbus: IFC version 1.3, 8 banks
Switched to clocksource timebase
NET: Registered protocol family 2
TCP established hash table entries: 512 (order: 0, 4096 bytes)
TCP bind hash table entries: 512 (order: 1, 8192 bytes)
TCP: Hash tables configured (established 512 bind 512)
UDP hash table entries: 256 (order: 1, 8192 bytes)
UDP-Lite hash table entries: 256 (order: 1, 8192 bytes)
NET: Registered protocol family 1
RPC: Registered named UNIX socket transport module.
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
futex hash table entries: 2048 (order: 5, 131072 bytes)
audit: initializing netlink subsys (disabled)
audit: type=2000 audit(1.552:1): initialized
HugeTLB registered 4 MB page size, pre-allocated 0 pages
HugeTLB registered 16 MB page size, pre-allocated 0 pages
HugeTLB registered 64 MB page size, pre-allocated 0 pages
HugeTLB registered 256 MB page size, pre-allocated 0 pages
HugeTLB registered 1 GB page size, pre-allocated 0 pages
NFS: Registering the id_resolver key type
Key type id_resolver registered
Key type id_legacy registered
ntfs: driver 2.1.32 [Flags: R/O].
jffs2: version 2.2. (NAND) 漏 2001-2006 Red Hat, Inc.
async_tx: api initialized (async)
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
console [ttyS0] disabled
serial8250.0: ttyS0 at MMIO 0xffe11c500 (irq = 36, base_baud = 18748125) is a 16550A
console [ttyS0] enabled
console [ttyS0] enabled
bootconsole [udbg0] disabled
bootconsole [udbg0] disabled
serial8250.0: ttyS1 at MMIO 0xffe11c600 (irq = 36, base_baud = 18748125) is a 16550A
serial8250.0: ttyS2 at MMIO 0xffe11d500 (irq = 37, base_baud = 18748125) is a 16550A
serial8250.0: ttyS3 at MMIO 0xffe11d600 (irq = 37, base_baud = 18748125) is a 16550A
ePAPR hypervisor byte channel driver
brd: module loaded
loop: module loaded
st: Version 20101219, fixed bufsize 32768, s/g segs 256
fsl-sata ffe220000.sata: Sata FSL Platform/CSB Driver init
scsi host0: sata_fsl
ata1: SATA max UDMA/133 irq 68
fsl-sata ffe221000.sata: Sata FSL Platform/CSB Driver init
scsi host1: sata_fsl
ata2: SATA max UDMA/133 irq 69
fe8000000.nor: Found 1 x16 devices at 0x0 in 16-bit bank. Manufacturer ID 0x000089 Chip ID 0x00227e
Amd/Fujitsu Extended Query Table at 0x0040
Amd/Fujitsu Extended Query version 1.3.
number of CFI chips: 1
nand: No NAND device found
fsl_espi ffe110000.spi: cs=0, init_csmode=0x100008
m25p80 spi32766.0: unrecognized JEDEC id bytes: ff, ff, ff
fsl_espi ffe110000.spi: at 0x80000800809be000 (irq = 53)
libphy: Fixed MDIO Bus: probed
libphy: Freescale XGMAC MDIO Bus: probed
libphy: Freescale XGMAC MDIO Bus: probed
libphy: Freescale XGMAC MDIO Bus: probed
libphy: Freescale XGMAC MDIO Bus: probed
libphy: Freescale XGMAC MDIO Bus: probed
libphy: Freescale XGMAC MDIO Bus: probed
libphy: Freescale XGMAC MDIO Bus: probed
libphy: Freescale XGMAC MDIO Bus: probed
libphy: Freescale XGMAC MDIO Bus: probed
libphy: Freescale XGMAC MDIO Bus: probed
cpu7/24: > WARNING (FM) [CPU07, /home/any888/QorIQ-SDK-V2.0-20160527-yocto/build_t2080rdb-64b/tmp/work-shared/t2080rdb-64b/kernel-source/drivers/net/ethernet/freescale/sdk_fman/Peripherals/FM/fm.c:3547 FM_Init]:
cpu7/24: Hack: No FM reset!
cpu7/24:
Freescale FM module, FMD API version 21.1.0
Qman ErrInt: Corenet Initiator Data Error
Freescale FM Ports module
fsl_mac: fsl_mac: FSL FMan MAC API based driver
fsl_mac ffe4e0000.ethernet: FMan MEMAC
fsl_mac ffe4e0000.ethernet: FMan MAC address: 00:04:9f:02:00:fd
fsl_mac ffe4e2000.ethernet: FMan MEMAC
fsl_mac ffe4e2000.ethernet: FMan MAC address: 00:04:9f:02:01:fd
fsl_mac ffe4e4000.ethernet: FMan MEMAC
fsl_mac ffe4e4000.ethernet: FMan MAC address: 00:04:9f:02:02:fd
fsl_mac ffe4e6000.ethernet: FMan MEMAC
fsl_mac ffe4e6000.ethernet: FMan MAC address: 00:04:9f:02:03:fd
fsl_mac ffe4f0000.ethernet: of_get_mac_address(/soc@ffe000000/fman@400000/ethernet@f0000) failed
fsl_mac: probe of ffe4f0000.ethernet failed with error -22
fsl_mac ffe4f2000.ethernet: of_get_mac_address(/soc@ffe000000/fman@400000/ethernet@f2000) failed
fsl_mac: probe of ffe4f2000.ethernet failed with error -22
fsl_dpa: FSL DPAA Ethernet driver
fsl_advanced: FSL DPAA Advanced drivers:
fsl_proxy: FSL DPAA Proxy initialization driver
fsl_proxy-proxy fsl,dpaa:ethernet@0: probed MAC device with MAC address: 00:04:9f:02:00:fd
fsl_proxy-proxy fsl,dpaa:ethernet@1: probed MAC device with MAC address: 00:04:9f:02:01:fd
fsl_proxy-proxy fsl,dpaa:ethernet@2: probed MAC device with MAC address: 00:04:9f:02:02:fd
fsl_proxy-proxy fsl,dpaa:ethernet@3: probed MAC device with MAC address: 00:04:9f:02:03:fd
fsl_proxy-proxy fsl,dpaa:ethernet@9: dev_get_drvdata(ffe4f2000.ethernet) failed
fsl_proxy-proxy: probe of fsl,dpaa:ethernet@9 failed with error -22
fsl_dpa_shared: FSL DPAA Shared Ethernet driver
fsl_dpa_shared-shared fsl,dpaa:ethernet@8: dev_get_drvdata(ffe4f0000.ethernet) failed
fsl_dpa_shared-shared: probe of fsl,dpaa:ethernet@8 failed with error -22
fsl_dpa_macless: FSL DPAA MACless Ethernet driver
Qman ErrInt: Corenet Initiator Data Error
fsl_dpa_macless: fsl_dpa_macle

0 件の賞賛
返信
3 返答(返信)

2,687件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Louche lou,

Would you please provide your Kernel configuration file and dts file?


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,688件の閲覧回数
qwertyuiop
Contributor I

We resolved this issue.

Thanks for your reply

0 件の賞賛
返信

2,688件の閲覧回数
renanqiang
Contributor I

Hi Louche,

I also have this problem on our board as you posted, could you share your method of fix this problem? 

Thanks very much.

0 件の賞賛
返信