T2080 - IBIS file for SI simulation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T2080 - IBIS file for SI simulation

2,743 Views
manikumar
Contributor II

Hi,

For pre layout simulation for T2080 processor please share IBIS file (For simulating of Hyperlynx SI)

Regards,

Mani

0 Kudos
Reply
2 Replies

2,452 Views
andrei_skok
NXP Employee
NXP Employee

I see you have open SR 1-3731611686 with the same question. Our engineer will provide you the T2080 IBIS-AMI model to simulate fast interfaces.

Please note, this model can be provided under NDA only.

0 Kudos
Reply

1,882 Views
Louis_Poitras
Contributor II

I also would like to receive the T2080 IBIS model. 

Renesas Electronics America has a NDA with NXP.

- Lou Poitras

0 Kudos
Reply