T1042's DDR4 Chip Select CS0_n not properly asserting.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

T1042's DDR4 Chip Select CS0_n not properly asserting.

3,481 次查看
trevorfox
Contributor III

Hi I am trying to bring up a custom board that uses a T1042 and five (5) component DDR4 memory IC's. These are 16 Gb x16 chips, making a 72 bit wide interface. Only one chip select used (CS0_n)

An odd thing is happenning - when I run the script loaded through a SW probe, the T1042 should be running its DDR4 calibration routine. It seems like it's starting, but, the chip select to the DDR4 from T1042 only asserts low for a couple nanoseconds and then immediately goes high. This process repeats indefinitely until I either power off the board, or assert a POR to the T1042.

This is clearly not correct behavior for the chip select, based on seeing the operation of the Dev Board D4RDB board - so the DDR4 on my board of course never functions.

Any ideas? I've verified the DC power stays at the required 1.2V +/- 50 mV.

0 项奖励
回复
7 回复数

3,415 次查看
yipingwang
NXP TechSupport
NXP TechSupport

You need to run DDRv tool to examine and bring up the DDR interface.

0 项奖励
回复

3,213 次查看
trevorfox
Contributor III

Hi Yipingwang,

 

I have received and run the DDRv tool, and it's failing with the following error.

"Error configuring target! - DDR initialization failed: D_INIT was not cleared by hardware!"

How do you suggest I proceed?

Trevor

0 项奖励
回复

3,206 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Would you please create a new thread to describe how you used QCVS DDRv tool?

0 项奖励
回复

3,412 次查看
trevorfox
Contributor III

Hi Yipingwang

Where do I get this DDRv tool?

 

Trevor

0 项奖励
回复

3,381 次查看
yipingwang
NXP TechSupport
NXP TechSupport

I assume that you have purchased Specialist Level CodeWarrior license.

Please login in www.nxp.com, please download QCVS for PA 4.5 from My NXP Account ->Software Licensing and Support->View accounts->NXP Software->QorIQ Configuration and Validation Enablement Suite -> 4.5 QCVS offline installation packages for CodeWarrior for Power Architectures Rev 4.5

Please download and install CodeWarrior 10.5.1 from My NXP Account ->Software Licensing and Support->View accounts->CodeWarrior Networked Suite - Specialist Level->10.5.1 CodeWarrior for Power Architecture - Professional Edition (Eclipse-Windows hosted)

Please install CodeWarrior for PA 10.5.1 first, then open CodeWarrior IDE and install QCVS(DDRv) tool from Help->Install New Software->Add->Archive.

 

 

0 项奖励
回复

3,347 次查看
trevorfox
Contributor III

Hi

I have not purchased this that I know of.

Is there a way to use this DDRv tool without the specialist level codewarrior license?

How do I purchase a "specialist level codewarrior license"?

 

Trevor

0 项奖励
回复

3,302 次查看
yipingwang
NXP TechSupport
NXP TechSupport
0 项奖励
回复