T1040RDB-PC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

T1040RDB-PC

2,239件の閲覧回数
kevinmcconnon
Contributor I

What is the difference between a  T1040RDB-PC and a T1040D4RDB-PA?

Thanks to a previous request, I understand that the D4 means that DDR4 memory is used and that the -Px suffix denotes a version.

WindRiver has told me that they have a BSP for a T1040RDB-PC, but what I find to be currently available is the T1040D4RDB-PA. I'm trying to determine specific differences so I can provide to them to determine if their BSP will work (we're using VxWorks and will use a WindRiver bootloader and BSP). Is there a way to find specific differences between the two boards such as replacement of components with "equivalent" parts?

0 件の賞賛
返信
3 返答(返信)

2,114件の閲覧回数
ufedor
NXP Employee
NXP Employee

Main difference is in SDRAM implementation:

T1040RDB - DDR3L UDIMM

T1040D4RDB - DDR4 UDIMM

0 件の賞賛
返信

2,114件の閲覧回数
kevinmcconnon
Contributor I

Thanks for the response. Is there anyway to get any more details? I've been told by WindRiver that sometimes even just a new version (just a difference in the suffix) can cause issues where adjustments to the BSP are needed for new components or what are considered to be extremely minor updates to the board.

Thanks again;

Kevin

0 件の賞賛
返信

2,114件の閲覧回数
ufedor
NXP Employee
NXP Employee

Please create a Technical Case:

https://community.nxp.com/thread/381898 

0 件の賞賛
返信