T1024 MII interfaces

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T1024 MII interfaces

1,371 Views
safeerkt
Contributor II

Hi,

We are using T1024 processor for one of our industrial application device where we already have a P1021 based previous revision. The main interfaces in the board are Ethernet and Ethercat.In P1021 based board we have used MII and RMII as MAC interface where we need 100BASE T signals.But in T1024 we could not find any other MII interfaces other than RGMII and SGMII where all are Gigabit outputs.Is there any way to configure the existing RGMII to low speed RMII or MII to use only 2 differential twisted pairs?

Many Thanks,

Safeer

0 Kudos
Reply
1 Reply

1,251 Views
alexander_yakov
NXP Employee
NXP Employee

There is no way to configure RGMII interface to lower speed MII or RMII, sorry.


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply