T1024 MII interfaces

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

T1024 MII interfaces

1,345件の閲覧回数
safeerkt
Contributor II

Hi,

We are using T1024 processor for one of our industrial application device where we already have a P1021 based previous revision. The main interfaces in the board are Ethernet and Ethercat.In P1021 based board we have used MII and RMII as MAC interface where we need 100BASE T signals.But in T1024 we could not find any other MII interfaces other than RGMII and SGMII where all are Gigabit outputs.Is there any way to configure the existing RGMII to low speed RMII or MII to use only 2 differential twisted pairs?

Many Thanks,

Safeer

0 件の賞賛
返信
1 返信

1,225件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

There is no way to configure RGMII interface to lower speed MII or RMII, sorry.


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信