SRIO for P2040 processor

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SRIO for P2040 processor

ソリューションへジャンプ
6,605件の閲覧回数
gouravjain
Contributor IV

Hey guys,

Its being first time do dealt with P2040 for me. Can any body has any docs related to SRIO part of this processor. your help would be highly appreciated. thanks in advance.

rgds,

Gourav

0 件の賞賛
返信
1 解決策
5,977件の閲覧回数
bpe
NXP Employee
NXP Employee

Direct links to the SRA-related software section on Freescale Infocenter,

Kernel driver:

http://www.freescale.com/infocenter/topic/QORIQSDK/3113236.html

USDPAA Application:

http://www.freescale.com/infocenter/topic/QORIQSDK/2918236.html

Both  the kernel driver and the userspace application are valid for P2040

The resource the links above point to is sometimes slow to answer. If you see

some error messages instead of the page, keep refreshing.

Harwdare-level details on DPAA Serial RapidIO Mesage Manager (SRA) can be found

in DPAARM, Chapter 10.


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
8 返答(返信)
5,977件の閲覧回数
vakulgarg
NXP Employee
NXP Employee

Have you checked P2040 reference manual?

0 件の賞賛
返信
5,977件の閲覧回数
gouravjain
Contributor IV

Hi Vakul,

yes i am referring that doc also. could you pls share any fruitful link with me if you have....your help would be much appreciated.

rgds,

Gourav

0 件の賞賛
返信
5,977件の閲覧回数
vakulgarg
NXP Employee
NXP Employee

Hi Gaurav

I not sure what kind of document you are looking for?

Do you want to see some manual or sample app running?

You can look at www.freescale.com/infocenter.

Search for SRIO there.

Let me know if this helps.

regards

Vakul

0 件の賞賛
返信
5,977件の閲覧回数
gouravjain
Contributor IV

Hi Vakul,

yes, I am looking for application note/manual on how to bring up SRIO for P2040 device.

thanks

rgds,

Gourav

0 件の賞賛
返信
5,977件の閲覧回数
vakulgarg
NXP Employee
NXP Employee

Do you want to use SRIO from user space application?

You can look at www.freescale.com/infocenter.


We provide a user space app named 'SRA' to demonstrate SRIO usage.

5,977件の閲覧回数
gouravjain
Contributor IV

Not able to open that link.

Can you post exact link for SRA??? Is it related to P2040 device???

0 件の賞賛
返信
5,978件の閲覧回数
bpe
NXP Employee
NXP Employee

Direct links to the SRA-related software section on Freescale Infocenter,

Kernel driver:

http://www.freescale.com/infocenter/topic/QORIQSDK/3113236.html

USDPAA Application:

http://www.freescale.com/infocenter/topic/QORIQSDK/2918236.html

Both  the kernel driver and the userspace application are valid for P2040

The resource the links above point to is sometimes slow to answer. If you see

some error messages instead of the page, keep refreshing.

Harwdare-level details on DPAA Serial RapidIO Mesage Manager (SRA) can be found

in DPAARM, Chapter 10.


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
5,977件の閲覧回数
gouravjain
Contributor IV

Thanks BPE and Vakul for your kind support :smileyhappy:

0 件の賞賛
返信