SATA SSD Detection Error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SATA SSD Detection Error

6,149件の閲覧回数
krishnaraj_d
Contributor I

Hi,

I am using P2040 Processor with Linux-3.8.13-rt9 which comply with Serial ATA 2.6 specification.  I was using SATA1 port of processor to plug in external 128GB SSD. Recently higher memory requirement came for 512 GB or above. When the 512 GB is plugged in the place of 128GB , it is not working. Errors where shown on the device boot up.

 

Both SSD are of same make, but 128GB supports SATA2 and 512GB supports SATA3. I guess SATA3 is backward compliant. I have checked the 512GB SSD  in a Ubuntu14.0 PC and it is getting detected properly. From the error log, I could find that the device is getting is detected with its size. But due to some reason, Linux is not able to mount it. Whether the size(512GB) could be the reason? If there are any pointers someone could provide, it would be awesome.

The relevant booting messages are copied below.

ata1.00: ATA-9: 2.5" SATA SSD 3MG2-P, M140815, max UDMA/133

ata1.00: 968959152 sectors, multi 1: LBA48 NCQ (depth 16/32)

ata1.00: failed to read native max address (err_mask=0x1)

ata1.00: HPA support seems broken, skipping HPA handling

ata1.00: configured for UDMA/133

scsi 0:0:0:0: Direct-Access     ATA      2.5" SATA SSD 3M M140 PQ: 0 ANSI: 5

sd 0:0:0:0: [sda] 968959152 512-byte logical blocks: (496 GB/462 GiB)

sd 0:0:0:0: [sda] Write Protect is off

sd 0:0:0:0: Attached scsi generic sg0 type 0

sd 0:0:0:0: [sda] Write cache: enabled, read cache: enabled, doesn't support DPO or FUA

ip_tables: (C) 2000-2006 Netfilter Core Team

TCP: cubic registered

Initializing XFRM netlink socket

NET: Registered protocol family 10

ip6_tables: (C) 2000-2006 Netfilter Core Team

sit: IPv6 over IPv4 tunneling driver

NET: Registered protocol family 17

NET: Registered protocol family 15

8021q: 802.1Q VLAN Support v1.8

Key type dns_resolver registered

fsl_dpa_macless: FSL DPAA MACless Ethernet driver ()

rtc-ds1307 0-0068: setting system clock to 2016-01-08 15:57:46 UTC (1452268666)

ata1.00: exception Emask 0x0 SAct 0x1 SErr 0x180000 action 0x6 frozen

ata1: SError: { 10B8B Dispar }

ata1.00: failed command: READ FPDMA QUEUED

ata1.00: cmd 60/08:00:00:00:00/00:00:00:00:00/40 tag 0 ncq 4096 in

          res 40/00:00:00:00:00/00:00:00:00:00/00 Emask 0x4 (timeout)

ata1.00: status: { DRDY }

ata1: hard resetting link

ata1: Hardreset failed, not off-lined 0

ata1: Signature Update detected @ 504 msecs

ata1: SATA link up 3.0 Gbps (SStatus 123 SControl 300)

ata1.00: configured for UDMA/133

ata1.00: device reported invalid CHS sector 0

ata1: EH complete

ata1.00: NCQ disabled due to excessive errors

ata1.00: exception Emask 0x0 SAct 0x1 SErr 0x180000 action 0x6 frozen

ata1: SError: { 10B8B Dispar }

ata1.00: failed command: READ FPDMA QUEUED

ata1.00: cmd 60/08:00:00:00:00/00:00:00:00:00/40 tag 0 ncq 4096 in

          res 40/00:00:00:00:00/00:00:00:00:00/00 Emask 0x4 (timeout)

ata1.00: status: { DRDY }

ata1: hard resetting link

ata1: Hardreset failed, not off-lined 0

ata1: Signature Update detected @ 504 msecs

ata1: SATA link up 3.0 Gbps (SStatus 123 SControl 300)

ata1.00: failed to IDENTIFY (I/O error, err_mask=0x40)

ata1.00: revalidation failed (errno=-5)

ata1: hard resetting link

ata1: Signature Update detected @ 504 msecs

ata1: SATA link up 3.0 Gbps (SStatus 123 SControl 300)

ata1.00: configured for UDMA/133

ata1.00: device reported invalid CHS sector 0

ata1: EH complete

0 件の賞賛
返信
5 返答(返信)

5,143件の閲覧回数
surendradhobale
Contributor III

Hello Yiping/Krishnaraj,

     I have T1040 RDB. I am looking to use SSD on SATA 2.0 interface. Could you recommend some SSD (128GB/256GB)  which is compatible with T1040. That will be very helpful.

Because I am looking to purchase SSD from market. If anyone already using working SSD. Please give me the details of the manufacturer.

Thanks in advance.

Reagards,

Surendra

0 件の賞賛
返信

5,143件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Krishnaraj,

I think this problem is caused by P2040 SATA controller incompatible with your SATA 3.0 512M device. You need choose SATA device which is available to switch to SATA 2.0(3Gbps).

The following is P2040 SATA controller features.

• Designed to comply with Serial ATA 2.6 Specification

• Supports speeds: 1.5 Gbps (first-generation SATA), 3 Gbps (second-generation

SATA)


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

5,143件の閲覧回数
krishnaraj_d
Contributor I

Hello Yiping,

Thank you for the reply.

I too doubted the SATA SSD. But I have two confusing points

a) On a Linux PC with 3Gbps interface, I didn't face any issue. SSD was getting loaded without any error.  Also I read that SATA3.0 is backward compatible with SATA2.0. So that shall not be an issue.

b) I tried Loading an HDD 6Gbps in the same slot which worked without error.

Could you recommend some SSD (512GB/1TB)  which is compatible with P2040. That will be very helpful.

Best Regards

Krishnaraj

0 件の賞賛
返信

5,143件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Krishnaraj,

Backward compatiblity means that SATA 3.0(6Gb/s) hosts and drives will operate when connecting a 3GB/s or 1.5G/s drives and hosts, by automatically dropping to the appropriate transfer rates.

So please confirm with the SDD producer whether their drives can be connected to all SATA 2.0 hosts(including P2040).


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

5,143件の閲覧回数
krishnaraj_d
Contributor I

Hi Yiping,

I have checked with the manufacturer. They told that SSD can work with SATA2.0 hosts.

Then in order to confirm this, with the help of manufacturer I have downgraded the SSD firmware to force SATA2. Once the SSD is made SATA2, it worked with P2040 without any issues.

Have a nice day,

Krishnaraj

0 件の賞賛
返信