Reboot Command Does Not Work In Custom P2020RDB Card

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Reboot Command Does Not Work In Custom P2020RDB Card

1,200件の閲覧回数
vidyasagartata
Contributor II

Dear All,

I am working the custom P2020-RDB board, reboot command does not work.

Please let me know what could could be problem.

Thanks,

Vidya

0 件の賞賛
返信
3 返答(返信)

1,044件の閲覧回数
vidyasagartata
Contributor II

Hi Alexander,

1. What do you mean by "custom P2020-RDB board" - what is the difference in comparison with original P2020-RDB from NXP?

We have designed the P2020 custom board, there is no difference in P2020-RDB and custom P2020 board.

2. Have you tried to run the same Linux on original P2020-RDB board and issue the same "reboot" command - what is the result?

Yes i am running the same Linux P2020-RDB, no there is no such issue in the P2020-RDB, but in custom P2020 design we are facing the issue.

Please how we can resolve the issue.

Thanks,

Vidya

0 件の賞賛
返信

1,044件の閲覧回数
vidyasagartata
Contributor II

Dear All,

I am working the custom P2020-RDB board, reboot command does not work.

Please let me know what could could be problem.

Please find the log below:

root@p2020rdb:/# reboot

INIT: Sending processes the TERM signal

INIT:Stopping Dropbear SSH server: stopped /usr/sbin/dropbear (pid 1776)

dropbear.

Stopping system message bus: dbus.

hwclock: can't open '/dev/misc/rtc': No such file or directory

Stopping network benchmark server: netserverstopped /usr/sbin/netserver (pid 1783)

.

Stopping system log daemon...0

Stopping kernel log daemon...0

Stopping internet superserver: xinetd.

Deconfiguring network interfaces... done.

Sending all processes the TERM signal...

Sending all processes the KILL signal...

Unmounting remote filesystems...

Deactivating swap...

Unmounting local filesystems...

Rebooting... reboot: Restarting system

After that board hangs up, please let me know what is the cause.

Thanks,

Vidya

0 件の賞賛
返信

1,044件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

1. What do you mean by "custom P2020-RDB board" - what is the difference in comparison with original P2020-RDB from NXP?

2. Have you tried to run the same Linux on original P2020-RDB board and issue the same "reboot" command - what is the result?


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信